Install the Historian Excel Add-in Using the Installer

Before you begin

Install one of the following 32-bit or 64-bit Microsoft® Excel® applications:
  • Microsoft® Excel® 2021 (32 & 64 bit)
  • Microsoft® Excel® 2019 (32 & 64 bit)
  • Microsoft® Excel® 2016 (32 & 64 bit)
  • Microsoft® Excel® 2013 (32 & 64 bit)

About this task

This topic describes how to install Excel Add-In using the installer. You can also install it at a command prompt.

Procedure

  1. Run the InstallLauncher.exe file. Contact the AWS support team for the installer.
  2. Select Historian Excel Add-in.
    The installer runs through the installation steps.
    Note: If using certain versions of Windows (like Windows 10 or Windows 2019), you may receive an error message, stating that some of the DLL files are not registered. You can ignore these messages.
  3. When prompted to reboot your system, select Yes.

Results

Excel Add-In is installed.

What to do next

Activate Excel Add-In.