Supported SELECT Statements Syntax
SELECT
statements allow you to retrieve data from the Historian
database for reporting and analysis. The SELECT
statements that the
OLE DB provider supports follow standard SQL-92 conventions. You can use SELECT
statements to retrieve information from any of the columns in any of the Historian
tables. The SELECT
statement returns a snapshot of data at the
given time of the query.
The order that you specify the columns in the SELECT
statement controls how the data is returned. For more information on the tables and each of the columns in each table, refer to Historian Database Tables .
Copy of
5vkn391s.Simulation00001
tag from the ihTrend
table, use the following query: SELECT "Copy of 5vkn391s.Simulation00001"
from ihTrend.- WHERE Clauses
- You can use a
WHERE
clause to specify search conditions in aSELECT
statement. You can specify a condition for any column in the table using theWHERE
clause.For example, you can search all rows of data in the ihTags table, where the
DataType
column equalsSingleFloat
. In another instance, you can find all tags that belong to a particular collector. Or, you can search for all tags with a certain poll rate, or range of poll rates, or ones with polling disabled.You can provide maximum 200 conditions in a
SELECT
statement.For more information on the columns for each individual Historian table, refer to Historian Database Tables.
Example 1: Search for All Single Float TagsSELECT* FROM ihtags WHERE datatype=singlefloat
Example 2: Specify Query Parameters to Obtain String DataSELECT* FROM ihrawdata WHERE tagname=SimulationString00001 AND samplingmode=interpolated AND IntervalMilliseconds=1H
In this example, you change the
SamplingMode
column from the default value ofCalculated
toInterpolated
in order to retrieve string data.Example 3: Use a WHERE Clause to Specify a Time RangeSELECT* FROM ihmessages WHERE timestamp>bom
Example 4: Use a Complex WHERE Clause to Find All Tags With a Specific Name and Description PatternSELECT* FROM ihtags WHERE(tagname LIKE '*001*' AND description LIKE '*sim*') OR (tagname LIKE '*02*' AND (description LIKE '*sec*' OR description LIKE '*sim*')) AND (timestamptype=source OR timestamptype=collector)
For more information on building complex
WHERE
clauses, see Logical Operators and Parenthetical Expressions. - ORDER BY
-
If you do not specify
ORDER BY
, the output of the row order cannot be assumed. For example, if you want to order the rows returned from the ihCollectors table by theCollectorName
column, you must include that column name inORDER BY
.As a more common example, when requesting timestamps with data, use the
Timestamp
column withORDER BY
to ensure that the samples are sorted in order by time.ORDER BY
sorts the returned records by one or more specified columns in either ascending or descending order. By default, the ascending order is considered. You can order results by one or more columns. If you sort by multiple columns, the sorting priority begins with the first column listed in the query, and then the next column, and so on.Abbreviation Description ASC
Specifies that the values must be sorted in ascending order, from lowest value to highest value. DESC
Specifies that the values must be sorted in descending order, from highest value to lowest value. The OLE DB provider treats
Null
values as the lowest possible values. It processesORDER BY
before it performs anyRowCount
truncation.Example 1: Retrieve Collectors in Descending Order Sorted by the Collectorname ColumnSELECT * FROM ihcollectors ORDER BY collectorname DESC
Example 2: Retrieve Messages in Ascending Order Sorted by Timestamp and Other ColumnsSELECT * FROM ihmessages WHERE timestamp>='5-oct-2001 00:00:00' AND timestamp<='18-jan-2002 00:00:00' ORDER BY timestamp, topic, username, messagenumber, messagestring
- TOP
-
With the
TOP
predicate, you can limit the number of rows returned to a specified number or percentage of rows. And then, enter the rest of the query. Typically, you includeORDER BY
in the query to sort the rows in a specified order.When you select the top number or top percentage of rows, the returned value is limited by the
RowCount
. For instance, suppose you want the top 30 percent of rows from a query that can return a possible 10,000 rows, but theRowCount
is set to 1000. The percentage logic processes the 3000 rows first, then it reduces the number to 1000 rows, as specified byRowCount
. The final result returns 1000 rows, even though the top 30 percent is processed first. Use aSET
statement orWHERE
clause to change or disable theRowCount
behavior.Example 1: Return the Top 40 Tags in Alphabetical OrderSELECT TOP 40 * FROM ihtags ORDER BY Tagname
Example 2: Return the Top 10 Most Recent MessagesSELECT TOP 10 timestamp, topic, username, messagestring FROM ihmessages WHERE timestamp<Now ORDER BY timestamp DESC
Example 3: Return the Top 10 Percent, RowCount DisabledSET rowcount=0 SELECT TOP 10 PERCENT timestamp, topic, username, messagestring FROM ihmessages WHERE timestamp<Now ORDER BY timestamp DESC
- LIKE
-
Use the
LIKE
expression when searching for column data similar to a specified text string. By using wildcards, you can specify the text strings that you want to search. You can use the wildcard before and/or after the text that you want to search for. Use an asterisk (*) for multiple unknown characters in a search string. Use a question mark (?) for a single unknown character.Note: You can also use a percentage (%) to select all tags that contain a specific string in the tag name and an underscore (_) to select all tags when you are unsure of only one character in the tag name. You must enclose these wildcard characters in single quotes (for example,'%'
or'_'
) when you use them in Historian tag names, but do not use single quotes if you want them to be treated as wildcards in SQL.Example 1: Use LIKE With Multiple Character ReplacementSELECT * FROM ihtags WHERE tagname LIKE *.Simulation* ORDER BY tagname SELECT * FROM ihtags WHERE tagname LIKE %.Simulation%
Example 2: Use LIKE With Single Character ReplacementSELECT * FROM ihtags WHERE tagname LIKE MYSERVER.Simulation0000? ORDER BY tagname SELECT * FROM ihtags WHERE tagname LIKE MYSERVER.Simulation0000'_' ORDER BY tagname
- AS
-
Use
AS
when you want to control the name of an output column. You can useAS
in all columns and tables except the ihTrend table. In the ihTrend table, you can only useAS
with theTimeStamp
column.Example: Set the Output Column NameSELECT status, collectorname AS Name, collectortype, status AS 'The Status', collectordescription FROM ihcollectors
- DISTINCT
-
DISTINCT
eliminates duplicate rows when all columns are equal. Floating-point values, however, may not compare as expected, depending on the precision. For example, if the numbers to the right of the decimal point are not equal for all values, similar columns are not eliminated. The columns must be exactly equal to be eliminated.Example 1: Retrieve the Set of Unique Data Types Used in an ArchiveSELECT DISTINCT datatype FROM ihtags
Example 2: Retrieve the Set of Tags With Raw Data Samples on a Specific DateSELECT DISTINCT tagname FROM ihRawData WHERE samplingmode=rawbytime AND timestamp>='11/28/2001' AND timestamp<='11/29/2001'
- GROUP BY
-
GROUP BY
combines records with identical values in the specified field list into a single record. Then, you can compute an aggregate value for the grouped records. The aggregate column does not exist in the actual table. Another calculated column is created with the results.Example: Group Messages by User Name and TopicSELECT username, topic, COUNT(*) FROM ihmessages WHERE timestamp >= '1-dec-2001 00:00:00' AND timestamp <= '7-dec-2001 00:00:00' GROUP BY username, topic ORDER BY username, topic
- SQL Aggregate Functions
SQL aggregate functions perform a calculation on a set of values in a column and return a single value. For instance, when comparing multiple tags, you can retrieve the minimum (
MIN
) of the returned minimum values. You usually use aggregate functions with theGROUP BY
clause, but it is not required. For more information, see Group By.Table 1. Supported Aggregate Functions Function Description AVG
Returns the average of the values in a group. Null values are ignored. COUNT
Returns the number of items in a group. Null values are not ignored. MAX
Returns the maximum value in a group. Null values are ignored. MIN
Returns the minimum value in a group. Null values are ignored. SUM
Returns the sum of all the values in a group. SUM
can be used with numeric columns only. Null values are ignored.STDEV
Returns the statistical standard deviation of all values in a group. Null values are ignored. STDEVP
Returns the statistical standard deviation for the population for all values in a group. Null values are ignored. VAR
Returns the statistical variance of all values in a group. Null values are ignored. VARP
Returns the statistical variance for the population for all values in a group. Null values are ignored. STDEV, STDEVP, VAR, and VARP
If a variance is defined as the deviation from an average data set value, and N is the number of values in the data set, then the following equations apply:
VAR = (Sum of Variances)^2 / (N - 1) VARP = (Sum of Variances)^2 / (N) STDEV = SquareRoot (VAR) STDEVP = SquareRoot (VARP)
Example 1: Retrieve the Total Number of TagsSELECT COUNT(*) FROM ihTags
Example 2: Calculate Values for Multiple Tags
The following figure displays the results of this query. Note the column names (Sum of value, Avg of value, Min of value, and Max of value) returned for the calculated columns.FROM ihrawdata WHERE tagname LIKE '*0001*' AND timestamp>='28-dec-2001 00:00' AND timestamp<='29-dec-2001 00:00' AND samplingmode=interpolated AND intervalmilliseconds=1h GROUP BY tagname ORDER BY tagname
- Conversion Functions
-
The Historian OLE DB provider generally returns data with the
VARIANT
data type. Some OLE DB clients may not understandVARIANT
data, however, and will require the data to be returned as an integer, float, or string data type. To accommodate this, the OLE DB provider includes the functions described in the following table.Table 2. Conversion Functions Function Description to_double (column)
Converts the specified column to a double float data type. to_integer (column)
Converts the specified column to a single integer data type. to_string (column)
Converts the specified column to a string data type. Note:- You must edit the SQL statement manually to add conversion functions.
- You can also use the fully qualified column name (for example,
ihRawData.value
). - Conversion functions are not available in
WHERE
orJOIN (ON)
clauses. - Conversion functions cannot be used within aggregate functions.
Example: Convert Values to Double Floatselect timestamp, to_double(value), quality from ihRawData
- JOIN
A table join is an operation that combines rows from two or more tables. You can join as many tables as you want within one
JOIN
statement. When you use a tableJOIN
in aSELECT
statement, you must specify the column name and table when selecting the columns that you want to compare. The syntax for table joins follows standard SQL language format.Table 3. Supported Join Operations Supported Join Feature Description Inner Join Combines records from two tables whenever there are matching values. Left Join or Left Outer Join Returns all of the rows from the left (first) of two tables, even if there are no matching values for records in the right (second) table. Right Join or Right Outer Join Returns all of the rows from the right (second) of two tables even if there are no matching values for records in the left (first) table. Full Join or Outer Join Returns all rows in both the left and right tables. Any time a row has no match in the other table, SELECT
list columns from the other table contain null values. When there is a match between the tables, the entire result set row contains data values from the base tables.Cross Join Returns all rows from the left table. Each row from the left table is combined with all rows from the right table. Old Join syntax Simply selects columns from multiple tables using the WHERE
clause without using theJOIN
keyword.Table joins are a powerful tool when organizing and analyzing data. A few examples are included in this section. However, refer to the documentation for your third-party reporting software for more complete information on building more complex queries.
JOIN Operations Rules
The following rules apply when working with
JOIN
operations for the Historian OLE DB provider:- You cannot join a table with itself.
- You cannot join any table with the ihTrend or ihQuerySettings tables.
JOIN
statements in the following examples.Example 1: Perform an Inner Join to Retrieve Only Data With Associated CommentsSELECT d.timestamp, d.tagname, d.value, c.username, c.comment FROM ihrawdata d INNER JOIN ihcomments c ON c.tagname=d.tagname AND c.timestamp=d.timestamp WHERE d.tagname LIKE '*0001*' ORDER BY d.timestamp, d.tagname, c.username, c.comment
Example 2: Perform a Left Outer Join to Retrieve All Data With and Without CommentsSELECT d.timestamp, d.tagname, d.value, c.comment FROM ihrawdata d LEFT OUTER JOIN ihcomments c ON c.tagname=d.tagname AND c.timestamp=d.timestamp WHERE d.tagname LIKE '*0001*' ORDER BY d.timestamp, d.tagname
Example 3: Perform a Right Outer Join to Retrieve All Comments and Their Accompanying DataSELECT d.tagname, d.timestamp, d.value, c.comment FROM ihrawdata d RIGHT OUTER JOIN ihcomments c ON c.tagname=d.tagname AND c.timestamp=d.timestamp WHERE d.tagname LIKE '*0001*' ORDER BY d.tagname, d.timestamp
Example 4: Perform a Cross JoinSELECT * FROM ihCollectors CROSS JOIN ihArchives
Example 5: Perform a Cross Join (Older Syntax)SELECT ihTags.Tagname, iharchives.Filename FROM ihTags, ihArchives
Example 6: Join the ihMessages and ihArchives Tables
This example usesSET StartTime
before theSELECT
statement. TheSET
statement is necessary because the timestamp criteria inSELECT
do not narrow down the time range for the ihMessages table until after the results have been collected and the join takes place.SET starttime='1-jan-2000' SELECT a.starttime, a.endtime, m.* FROM ihmessages m JOIN iharchives a ON m.timestamp>=a.starttime AND m.timestamp<=a.endtime WHERE a.iscurrent=true
Example 7: Interleave Data and Messages by TimestampSELECT d.timestamp, m.timestamp, d.tagname, m.messagestring, d.value FROM ihRawData d FULL OUTER JOIN ihMessages m ON d.timestamp=m.timestamp WHERE d.tagname=simulation00001 AND d.timestamp>='30-nov-2001 00:00:00' AND d.timestamp<='06-dec-2001 00:00:00'
Example 8: Retrieve the Greatest Values Across All Simulation Tags
In the following example, we join theihRawData
andihTags
tables, because theihRawData
table does not contain theCollectorType
column.SELECT TOP 300 ihRawData.tagname, ihRawData.timestamp, ihRawData.value, ihRawData.Quality FROM ihRawData INNER JOIN ihTags ON ihRawdata.Tagname = ihTags.Tagname WHERE ihRawData.tagname LIKE simulation* AND ihRawData.timestamp>=11/28/2001 AND ihRawData.timestamp<=11/29/2001 AND ihRawData.samplingmode=interpolated AND ihRawData.intervalmilliseconds=1H AND ihTags.datatype!=FixedString AND ihTags.datatype!=variablestring AND ihRawData.quality>0 ORDER BY value DESC, timestamp DESC
Example 9: Join the ihComments and ihRawData TablesSET starttime='28-nov-2001 08:00', endtime='29-nov-2001 09:00', samplingmode=interpolated, intervalmilliseconds=6m SELECT d.tagname, d.timestamp, d.value, c.storedontimestamp, c.username, c.datatypehint, c.comment FROM ihcomments c FULL OUTER JOIN ihrawdata d ON c.tagname=d.tagname AND c.timestamp=d.timestamp WHERE d.tagname LIKE '*0001*' ORDER BY d.tagname, d.timestamp,c.storedontimestamp, c.datatypehint, c.username, c.comment
Example 10: Report by Tag Description
In the following example, we join theihRawData
andihTags
tables to get theDescription
column from theihTags
table.SELECT d.timestamp, t.description, d.value, d.quality FROM ihrawdata d INNER JOIN ihtags t ON d.tagname=t.tagname WHERE d.tagname LIKE '*0001' ORDER BY d.timestamp, t.description
Example 11: Join Three TablesSELECT ihTags.Tagname, ihTags.Description, ihRawData.TimeStamp, ihRawData.Value, ihRawData.SamplingMode, ihComments.Comment FROM ihTags ihTags, ihRawData ihRawData, ihComments ihComments WHERE ihTags.Tagname = ihRawData.Tagname AND ihRawData.Tagname = ihComments.Tagname AND ihRawData.Timestamp = ihComments.Timestamp AND ihRawData.TimeStamp >= {ts '2002-03-01 09:39:00.000'} AND ihRawData.TimeStamp <= {ts '2002-03-01 09:41:00.000'} AND ihRawData.SamplingMode = 'RawByTime' AND ihTags.Tagname LIKE '%TestTag1%'
Example 12: Perform a Right Join (Older Syntax)SELECT ihTags.Tagname, ihTags.CollectionInterval, ihCollectors.CollectorName, ihCollectors.DefaultCollectionInterval FROM ihTzzz|
Example 13: Perform a Left Join (Older Syntax)SELECT ihTags.Tagname, ihTags.CollectionInterval, ihCollectors.CollectorName, ihCollectors.DefaultCollectionInterval FROM ihTags ihTags, ihCollectors ihCollectors WHERE ihTags.CollectionInterval *=ihCollectors.DefaultCollectionInterval AND ihTags.Tagname LIKE '%TestTag%'
- Quotation Marks
-
You must use quotation marks when you specify a string that contains a space, a comma, or a reserved word. Reserved words are defined by the SQL-92 conventions. Single and double quotes are equivalent in queries.
Example: Use Quotes When a Text String Contains a SpaceSELECT * FROM ihtags WHERE comment LIKE 'alert message'
- Timestamp Formats
Timestamps appear not just in the
TimeStamp
columns, but also in columns such as theStartTime
,EndTime
, andLastModified
columns. You can use the date and/or time in a SQL statement that contains a timestamp. Valid date and time formats are as follows:- System short date and time.
- SQL date and time.
- ODBC date and time.
The time format for system short timestamps is the same as the time format defined in the Windows Control Panel.
When entering a query you should use a period as the decimal separator to separate seconds from milliseconds or microseconds.
When using the SQL date and time, you should always use the English abbreviations for the desired month.
If you enter only a start time, the end time is assumed to be now. For example, if you enter
starttime > yesterday
in aWHERE
clause, the end time for the query is now, even if you previously set an end time.If you enter only an end time, the start time is December 31, 1969, 19:00:00.001. If you use this as the start time, you can overload the Historian server and the provider. For example, if you use
Example 1: Use the System Short Date and Timetimestamp < now
, you might cause an overload.
Example 2: Use the SQL Date and TimeSET starttime='02/01/2002 11:00:00'
Example 3: Use the ODBC Date and TimeSET starttime='14-sep-2001 11:00:00'
Example 4: Set the Start Time to 4 AM TodaySET starttime={ts '2002-06-20 15:34:08'}
Example 5: Set the Start Time in MillisecondsSET starttime='04:00:00'
Example 6: Set the Start Time in MicrosecondsSET starttime='7/12/2011 12:03:16.183'
SET starttime='7/12/2011 12:03:16.178439'
- Date and Time Shortcuts
Example 1: Set the Start Time to the First Day of the MonthTime Segment Meaning now
Now (the time and date that you execute the query) today
Today at midnight yesterday
Yesterday at midnight mon
The previous Monday at midnight tues
The previous Tuesday at midnight wed
The previous Wednesday at midnight thurs
The previous Thursday at midnight fri
The previous Friday at midnight sat
The previous Saturday at midnight sun
The previous Sunday at midnight boy
First day of year at midnight eoy
Last day of year at midnight bom
First day of month at midnight eom
Last day of month at midnight
Example 2: Retrieve Messages Dated TodaySET starttime=bom
SELECT * FROM ihmessages WHERE timestamp>=today
- Relative Date and Time Shortcuts
-
Optionally, you can add or subtract relative time shortcuts to the absolute times.
Table 4. Relative Date and Time Shortcuts Time Segment Meaning s
Second m
Minute h
Hour d
Day w
Week micro
Microsecond You can use relative time shortcuts when defining time intervals. For instance, use these shortcuts when you specify a value for theExample 1: Set the Start Time to 10 Days Before Yesterday and End Time to TodayIntervalMilliseconds
column.Note: You cannot use relative time shortcuts to add or subtract microseconds to or from absolute times.
Example 2: Retrieve the Previous 24 Hours of MessagesSET starttime=yesterday-10d, endtime=today SELECT * FROM ihQuerySettings
Example 3: Select Data Starting at 1AM Yesterday and Ending NowSELECT * FROM ihMessages WHERE timestamp>=Now-24h
Example 4: Retrieve Raw Data With a 1 Hour (3600000 Milliseconds) Interval Between Returned SamplesSELECT * FROM ihrawdata WHERE timestamp>=yesterday+1h AND timestamp<=now
Example 5: Retrieve Raw Data With a 100 Microseconds Interval Between Returned SamplesSELECT * FROM ihrawdata WHERE intervalmilliseconds=1h
Example 6: Retrieve This Week's Output to DateSELECT * FROM ihrawdata WHERE intervalmilliseconds=100micro and starttime>= '7/12/2011 12:03:16.100000' and endtime<='
SET starttime=Sun, endtime=Now, intervalmilliseconds=1d, samplingmode=rawbytime SELECT tagname, SUM(value) FROM ihRawData WHERE tagname LIKE *00* GROUP BY tagname
- Comparison Operators
Table 5. Expression Comparisons Comparison Symbol Meaning <
Less Than >
Greater Than <=
Less Than or Equal >=
Greater Than or Equal =
Equal !=
Not Equal !>
Not Greater Than !<
Not Less Than BETWEEN x AND y
Between the values x
andy
inclusive, wherex
andy
are numeric valuesA literal on the left side of the comparison operator is not supported. For example, this statement would fail:SELECT DISTINCT tagname FROM ihRawData WHERE 50>Value
But the following statement succeeds since theExample 1: Retrieve Tags with a High EGU Greater Than 300Value
column is to the left of the>
operator:SELECT DISTINCT tagname FROM ihRawData WHERE Value>50
Example 2: Retrieve Tags with a Specific DescriptionSELECT DISTINCT tagname, loengineeringunits, hiengineeringunits FROM ihTags WHERE hiengineeringunits > 300
Example 3: Retrieve All Samples Where the Value Exceeds Query Supplied ValuesSELECT tagname, description FROM ihTags WHERE description = "aa"
Example 4: Retrieve All Samples Where the Value is Between Query Supplied ValuesSELECT timestamp, tagname, value FROM ihRawData WHERE samplingmode=rawbytime AND value>75
Example 5: Retrieve All Tag Names Starting with an A or BSELECT timestamp, tagname, value FROM ihRawData WHERE samplingmode=lab AND value BETWEEN 25 AND 75
SELECT * FROM ihtags WHERE tagname < 'C'
- Logical Operators
-
The following logic operators are supported:
AND
OR
NOT
Example 2: Use the OR Logical OperatorSELECT * FROM ihTags WHERE Tagname LIKE 'Simulation*' AND CollectionInterval<3000
Example 3: Use the NOT Logical OperatorSELECT * FROM ihTags WHERE Tagname LIKE 'ComputerName.Simulation*' OR tagname LIKE '*String*'
Example 4: Use the NOT Logical Operator With a LIKE ExpressionSELECT * FROM ihTags WHERE NOT Datatype=SingleFloat
SELECT * FROM ihTags WHERE Tagname NOT LIKE '*String*'
- Parenthetical Expressions
-
Parentheses control the order of evaluation of the logical operators in an expression. The OLE DB provider supports parentheses in a
Example 1: Use ParenthesesWHERE
clause. You can use multiple sets of parentheses, and nest parenthetical expressions.
Example 2: Use Parentheses with Logical Operators and TimestampsSELECT * FROM ihTags WHERE (tagname LIKE *001 AND description="aa") OR tagname LIKE *002
Example 3: Use Multiple Sets of ParenthesesSELECT * FROM ihRawData WHERE tagname=Simulation00001 AND (Timestamp=>Tu AND Timestamp<=Wed OR Timestamp>=Fri AND time
SELECT * FROM ihtags WHERE (tagname LIKE '*001*' AND description LIKE '*sim*') OR (tagname LIKE '*02*' AND (description LIKE '*sec*' OR description LIKE '*sim*'))