ihEnumeratedSets Table

The ihEnumeratedSets table contains information about enumerated sets that are defined in the system. The following table describes the columns of the ihEnumeratedSets table.

Table 1. ihEnumeratedSets Table
Column Name Data Type Description
SetName VT_BSTR The name of the set.
Description VT_BSTR The description of the set.
NumberofStates VT_I4 The number of states a set contains.
NumberofTagReferences VT_I4 The number of tags with which a set is associated.
SetDataType VT_BSTR The data type of the set.
AdministratorSecurityGroup VT_BSTR The security group to which the set belongs.
LastModifiedUser VT_BSTR Indicates which user last modified the set.
LastModifiedTime VT_DBTimeStamp Indicates the last time the set was modified.
RowCount VT_I4 Indicates the maximum number of rows that can be returned. A value of 0 indicates that there is no limit to the number of rows returned.

ihEnumeratedSets Examples

Sample SQL statements for the ihEnumeratedSets table are outlined in the following examples.

Example 1: Retrieve All Sets By Using Integer States

SELECT * FROM ihEnumeratedSets
WHERE SetDataType=’integer’

Example 2: Retrieve a Set By Name From Sets

SELECT * FROM ihEnumeratedSets
WHERE setname like PLC1