Upgrade Collectors
Before you begin
- Direct upgrades from a previous version of Cloud Collectors to Historian 2024 Collectors is not supported. It is recommended that you uninstall the older version of collectors and re-install the Historian 2024 Collectors from the Historian 2024 install media (.ISO).
- If an iFIX collector instance created in version 9.0 exists, after you upgrade collectors, another instance of the iFIX collector is created. Because of this, the Remote Collector Manager (RCM) will not work correctly. Therefore, if you want to use RCM, you must delete one of the instances. If needed, you can manually create another instance of the iFIX collector using Configuration Hub or the RemoteCollectorConfigurator utility. This is applicable to the iFIX Alarms and Events collector as well.
- For collectors earlier than version 7.1, additional registries that you create manually are deleted. Therefore, we recommend that you back them up, uninstall the collectors, and then install the latest version.
Procedure
Install the
collectors.
The collectors are upgraded to the latest version.