General Parameters of a Collector
This topic provides a list of general parameters that are applicable to each type of collector.
Collector Type | Applicable General Parameters |
---|---|
The Calculation collector |
|
The CygNet collector |
|
The iFIX Alarms and Events collector | General1 - optional. Used for ProgId. Default value: Proficy.OPCiFIXAE.1 |
The iFIX collector |
|
The MQTT collector |
|
The ODBC collector |
|
The OPC Classic Alarms and Events collector | General1 - required. Used for the OPC source server progID. |
The OPC Classic DA collector | General1 - required. Used for the OPC source server progID. |
The OPC Classic HDA collector |
|
The OPC UA DA collector |
|
The OSI PI collector |
|
The OSI PI distributor |
|
The Python Collector |
|
The Server-to-Server distributor |
|
The Windows Performance collector | None |
The Wonderware collector |
|