Access Events
About this task
- The amount of tag data fetched from Data Archiver
An event is generated every hour in CloudTrail, containing the total number of data samples (in millions) that are fetched from Data Archiver in that hour.
For example, suppose you plot the trend chart of tag values in the past hour, and 1,045,000 samples are fetched from Data Archiver. In the event, the usageQuantity is set to1
(indicating 1 million), and the usageDimension is set toUnits_Queried
(indicating that this event is for fetching data from Data Archiver). The remaining 45,000 samples are added to the ones collected in the next hour. - The amount of tag data written to Data Archiver
An event is generated every hour, containing the total number of samples (in millions) that are written to Data Archiver.
For example, if you have 1000 tags, each one set to a resolution of 1 second, 3,600,000 data samples are written to Data Archiver per hour. In the event, usageQuantity is set to3
, and usageDimension is set toUnits_Stored
. The remaining 600,000 samples are added to the next hour. - The amount of tag data exported in bulk to Amazon S3 in the Parquet or CSV
file format
An event is generated every hour, containing the total number of samples (in millions) that are exported from Data Archiver to Amazon S3 in the Parquet or CSV file format.
For example, if 4,785,000 data samples are exported per hour, the usageQuantity is set to4
, and usageDimension is set toBulk_Export
. The remaining 785,000 samples are added to the next hour.
Events are also generated when Data Archiver is started or stopped.
Procedure
- Log in to the AWS console.
- Under CloudTrail. , select
- In the left section, select Event history.
-
Set the Event source to
metering-marketplace.amazonaws.com.A list of read/write/export events appears. If needed, you can filter the events for a specific duration.
-
Select the event whose details you want to access.
The Meter Usage page appears, displaying the event details. In the Event Record section, the usageDimension parameter indicates whether the event is for fetching, writing, or exporting data. The usageQuantity parameter contains the number of samples that are fetched, written, or exported in that duration.