Success = 0 | Operation successful. |
Failed = -1 | Operation failed. |
Timeout = -2 | Operation failed due to timeout. |
NotConnected = -3 | Not connected to Historian server. |
CollectorNotFound = -4 | The given collector does not exist on the server. |
NotSupported = -5 | Operation not supported. |
DuplicateData = -6 | Attempt to overwrite an existing data sample. |
InvalidUsername = -7 | Bad user name or password. |
AccessDenied = -8 | Insufficient permissions for operation. |
WriteInFuture = -9 | Attempted data write too far in the future. |
WriteArchiveOffline = -10 | Attempted data write to an offline archive. |
WriteArchiveReadonly = -11 | Attempted data write to a read-only archive. |
WriteOutsideActiveRange = -12 | Attempted data write beyond the configured active range. |
WriteNoArchiveAvailable = -13 | Attempted data write with no available archives. |
InvalidTagname = -14 | The requested tag was not found. |
LicensedTagCountExceeded = -15 | Number of licensed tags exceeded. |
LicensedConnectionCountExceeded = -16 | Number of licensed server connections exceeded. |
InternalLicenseError = -17 | Internal license error. |
NoValue = -18 | No available tag data. |
DuplicateCollector = -19 | The given collector name already exists on the server. |
NotLicensed = -20 | Server or feature is not licensed. |
CircularReference = -21 | Circular reference detected in calculation. |
BackupInsufficientSpace = -22 | Insufficient disk space to perform backup. |
InvalidServerVersion = -23 | Operation unsupported due to server version. |
QueryResultSizeExceeded = -24 | Upper limit on query results exceeded. |
DeleteOutsideActiveRange = -25 | Attempted data delete outside allowed modification interval. |
AlarmArchiverUnavailable = -26 | Alarms and Events subsystem unreachable. |
ArgumentException = -27 | A supplied argument is invalid. |
ArgumentNullException = -28 | A supplied argument is NULL. |
ArgumentOutOfRangeException = -29 | A supplied argument is outside the valid range. |
InvalidEnumeratedSet = -30 | The requested Enumerated Set was not found. |
InvalidDataStore = -31 | The requested data store was not found. |
NotPermitted = -32 | Operation not permitted. |
InvalidCustomDataType = -33 | The Custom data type is not supported. |
ihSTATUS_EXISTING_USERDEF_REFERENCES = -34 | N/A |
ihSTATUS_INVALID_TAGNAME_DELETEDTAG = -35 | N/A |
ihSTATUS_INVALID_DHS_NODENAME = -36 | N/A |
ihSTATUS_DHS_SERVICE_IN_USE = -37 | N/A |
ihSTATUS_DHS_STORAGE_IN_USE = -38 | N/A |
ihSTATUS_DHS_TOO_MANY_NODES_IN_MIRROR = -39 | N/A |
ihSTATUS_ARCHIVE_IN_SYNC = -40 | N/A |
InvalidArchiveName= -41 | N/A |
InvalidSession = 1 | Session id is invalid. |
SessionExpired = 2 | Session has expired. |
UnknownError = 3 | Unknown error, please check server log. |
NoValidClientBufferManager= 4 | No valid client buffer manager. |
NoValueInDataSet = 5 | No value in returned data set. |
TagNotExisting = 6 | Tag doesn't exist. |
ClientBufferManagerCommunicationError = 7 | Service call to central buffer server fail. |
TagTypeNotSupported=8 | Tag type is not supported. |
ValueTypeNotMatchTagDataType = 9 | Value type doesn't match tag data type. |
InvalidParameter=10 | Invalid query parameter. |
TagSearchResultIsHuge = 11 | Tag Search Criteria result was more than 5000. |
InvalidHistorianServer=12 | No valid server or historian server name isn't in the server list. |
ihSTATUS_INVALID_INTERFACETYPE = -49 |
The collector type is not valid. For a list of collector types,
refer to r_collector_type_and_subtype.html. |
ihSTATUS_INTERFACE_START_FAIL = -50 |
Starting the collector has failed. |
ihSTATUS_INTERFACE_STOP_FAIL = -51 |
Stopping the collector has failed. |