Mobile Application
About the GE Digital APM Mobile Application
APM provides a mobile app that can be installed on iOS, Android, and Windows devices.
This app offers certain APM functionality designed specifically for use offline and includes the following modules:
- Mobile Proof Testing
- Rounds Data Collection
- SIS Management
Note: Currently, Legacy GE Digital APM Mobile app for Windows application does not support GeoLocation feature during data collection. This feature will be re-enabled in the future releases.
Mobile Application Supported Operating Systems
Supported Operating Systems
Important:
- Any management policy applied to mobile devices must be set up to allow the required permissions for the APM mobile application. If restrictions are placed on iOS, Windows, or Android devices by a global policy or mobile device management system, device storage, scanning, photography, location services, and other functionality may be disabled.
- Ensure that the IP range of the mobile devices on which the APM mobile application is installed has been whitelisted.
- If you are using a Windows device, ensure that Windows App Store access is enabled.
- Ensure that the application is distributed to all relevant devices.
The following table lists the operating systems and corresponding versions that the APM mobile application supports.
Operating System | Version(s) Supported |
---|---|
iOS | 12, 13, and 14 |
Android | 10, 11, and 12 |
Windows | Windows 10 (64 bit) |
Note: The method used to access Reference Documents in the APM mobile application will vary depending on your device platform. For example, on Windows and Android devices, the first time you access Reference Documents, you will be prompted to select the application in which you want to open a file, and this selection will then become the default. Apple iOS will always prompt you to select an application.
Install the GE Digital APM Mobile Application on an iOS Device
GE Vernova provides an iOS app that can be downloaded from the App Store and installed on your iOS device.
Procedure
Install the GE Digital APM Mobile Application on an Android Device
GE Vernova provides an Android app that can be downloaded from the Google Play Store and installed on your Android device.
Procedure
Install the APM Mobile Application on a Windows Device
Procedure
Access APM via the Mobile Application
Before You Begin
If you are using an Android device, ensure that you have set up your device PIN prior to accessing the APM mobile application.
Procedure
Access APM via the Mobile Application while Offline
Before You Begin
- Sign in at least once while online.
- You must have an offline sign-in PIN, which is separate from your APM password.
Procedure
Reset Offline Sign-In PIN
Complete the following steps to reset your PIN for signing in to GE Digital APM mobile application while offline.
Before You Begin
- You must have already configured your offline sign-in PIN when you accessed the GE Digital APM mobile application for the first time.
- You must be online to reset your offline sign-in PIN.
About This Task
Note: If you are using an Android device on which you have configured a screen lock, if you remove the screen lock, you must reset your offline sign-in PIN for the GE Digital APM mobile application. For example, if your Android device previously required a password to unlock the screen but you changed the Screen lock setting to None, you must reset the offline sign-in PIN for the APM mobile application.