Windows Authentication Configuration

Windows authenticated users can use their Windows user name and password when logging into CIMPLICITY if they are members of selected Windows groups.

You can determine how long the application must wait before a connection timeout occurs when a connection to an LDAP server is not established. You can use the ADV_LDAP_CONNECT_TIMEOUT global parameter to set the timeout.

Do the following to select and configure the groups that CIMPLICITY will use for authentication.

Step Description
Step 1 Open the Windows Authentication window.
Step 2 List Windows groups in a selected domain.
Step 3 Select groups that will be authenticated for CIMPLICITY.
Step 4 Map a role for each group.
Step 5 Prioritize groups.
Step 6 Enable automatic log ins.
Step 7 Save or Cancel the Windows Authentication Configuration.