Point Attributes in CimEdit
Procedure
- Select or create an object to which the point attribute will be applied.
- Open the object's Properties dialog box.
-
Click the Edit Expression button
to the right of the Expression field that applies to the object's runtime behavior.
The Edit Expression dialog box opens.
-
Enter the Point ID and attribute you want to display using the following syntax.
'< POINT_ID>.<ATTRIBUTE_ID>'
Where
< POINT_ID> is the Point ID of any configured point
< ATTRIBUTE_ID> is one of the configuration attributes described in the point attributes documentation.
Important: You must enclose the syntax in single quotes, because the '.' character is a special character.Example: Point Attribute Configuration
- Open a Properties dialog box for a text object.
- Select Text.
-
Enter the following.
A Enter a default string in the String field. B Enter a '<POINT_ID>.<ATTRIBUTE_ID>' expression in the Expression field. Tip: Click the Expression Editor button to use the Expression Editor.C Click OK.
Results
The string displays as follows.
In CimEdit | In CimView |
---|---|
Point Attribute | %R456 |
Point Attribute Guidelines
- You can force an expression to return a numeric value, if the value is a number but the attribute is listed as returning a character. You use the operator VAL to do this.
Example
VAL('DEV1750.ALARM_HIGH')+VAL(DEV1900.ALARM_HIGH')
- Some of the attributes are specific to points of a particular type. Valid point types, which are specified in the attribute list, are:
- All (point types)
- Device
- Derived (Virtual)
- Global (Virtual)
- All field names and enumerated data are case insensitive.