BQM_Alr
BQM_Alr begins executing when the project starts.
BQM_ALR.exe:
- Is located in the CIMPLICITY process control.
- Picks the job from the directory and posts it to specific device.
- BQM_Alr debug file.
- BQM_Alr debug information.
BQM_Alr debug file
If
Debug_Bqma=1 is in debugbco.txt.
BQM_Alr
:
-
Generates a debug file named ErrorInBQM_ALR_<ProjectName>.err.
-
Places the file in c:\TEMP.
BQM_Alr Debug information
Information in ErrorInBQM_ALR_<ProjectName>.err includes:
Success conditions
Data about successfully printing and moving the job from the Active to the History folder is located after the statements.
- In GetCMAData
- In GetDevList
Failure conditions
Data about failure conditions includes:
- Missing data is located after the statements:
- GetCMAData
- GetDevList
- Search for token “PATH:” and the path should be <SpoolLocation>\<ProjectName>\ACTIVE\<DeviceName>.
Example
Path: C:\Temp\IBC1\Yane\Active\FINEPRINT1
- Search for tokens “pPrinterInfo->Status: ” & “pJob->Status: ”
If any one token is not 0, there is an Error State on the device.
- Search for token “No of GenFlds: ” & “No of TokensInFile: ”.
If the count does not match, the uob will be moved to an Invalid directory.