/keypad
For: CimView (and Webspace) only
Displays a keypad window on the user's screen whenever the user has to perform a Variable Setpoint action in a procedure. To enter a new setpoint value, the user clicks on the appropriate keys in the keypad window rather than entering them from a keyboard.
This option is only applied if it is used with the first CimView window opened. This window is known as the primary window. If used with subsequent open commands, it will be ignored.
Example
cimview /keypad C:\myproj\scr.cim
Important
- On some Windows 8 systems, keypad may not work well if the standard
/keypad
command line argument (above) is used. If this occurs aCimDesktop
utility can be used as the command and, in most instances, will display the keypad correctly.
The syntax is:
CimDesktop CimView /keypad c:\myproj\scr.cim
-
/captive
and/nomenutitle
are also currently supported when using this tool.