/dumppoints
For: CimEdit only
Loads each file and displays a dialog listing the points used in the file.
The dialog looks like this:

No CimEdit window is displayed, and CimEdit exits when done.
You can also use the Point View tab in the Screen Properties dialog to display the points currently used on a screen. In addition to displaying the list of points, the Point View tab will show you where they are used, and let you edit the Point IDs.
Note: Make sure to include in the command line the complete path to the file.
Example
cimedit.exe /dumppoints C:\myproj\myscreen.cim