Supercharge your GE solution! Download a free trial of Proficy Operations Hub, CSense analytics, and more. Explore our Proficy 2024 releases to find out more.
Important: You do not have the latest version of CIMPLICITY! You are missing out on the newest capabilities and enhanced security. For information on all the latest features, see the CIMPLICITY product page. For more information on upgrades, contact your GE Digital sales agent or e-mail GE Digital Sales Support. For the most up-to-date documentation, go here.
User Runtime Properties
About this task
You can use the User Setup dialog box to change the runtime user log in properties in your project.
Open the User Setup dialog box
Configure user runtime account access
Open the User Setup dialog box
Procedure
Do one of the following.
Select Project > Properties on the Workbench menu bar.
Select the Project Properties.
The Project Properties dialog box opens.
Select the Settings tab.
Select Users.
Select Settings.
The User Setup dialog box opens.
Configure user runtime account access
About this task
Automatic account disable
Password Complexity Rules
Automatic account disable
About this task
CIMPLICITY can be configured to automatically disable a user account after a selected number of failed log in attempts.
Procedure
Check one of the following.
No account disable
Disables automatic account disabling.
Users will be allowed unlimited log in attempts.
Account disable
Enables:
Automatic account disabling
Disable after n bad logon attempts box.
Enter the number of log in attempts that can fail before CIMPLICITY disables the account.
Users will be allowed the specified number of log in attempts. If the number is exceeded CIMPLICITY disables the user account and generates a $LOGIN_FAILURES event.
To re-enable the account, the system administrator needs to dynamically re-enable the user account.