Supercharge your GE solution! Download a free trial of Proficy Operations Hub, CSense analytics, and more. Explore our Proficy 2024 releases to find out more.
Important: You do not have the latest version of CIMPLICITY! You are missing out on the newest capabilities and enhanced security. For information on all the latest features, see the CIMPLICITY product page. For more information on upgrades, contact your GE Digital sales agent or e-mail GE Digital Sales Support. For the most up-to-date documentation, go here.
Reshape Objects
About this task
The Reshape tool is particularly useful for changing the shape of a polyline or polygon. Several keys on the keyboard and the CimEdit grid provide you with additional aids when you are reshaping the object.
Reshape tool
Object reshaping
Handles deleted or added
Reshape Tool
Procedure
Click Reshape in the Drawing>Edit group on the CimEdit Ribbon bar.
Select the object to reshape.
The object is surrounded by reshape handles.
Object Reshaping
The object handles can be moved in any direction.
As the object is reshaped, its handles remain connected to the same position that they were at on the original shape; that position may have changed location.
Drag any handle to continue reshaping the object.
A
A Transparent image displays how the object is being reshaped.
B
A contrasting shade of color displays the original object shape.
Release the left-mouse button.
Result: The object displays in its new shape.
Handles Deleted or Added
You can delete or add handles for polyline or polygon objects to further refine the reshaping.
Choose one of the following.
Press Ctrl on the keyboard.
Position the cursor at the edge of the object to be revised.
For a polyline or polygon, the cursor turns to a crosshair.
Do one of the following.
Click a vertex.
The vertex is deleted.
The line straightens between the vertex to the right and left of the deleted vertex.
Click a point in the line.
A vertex is added to the line in the location that was clicked..