Important: You do not have the latest version of CIMPLICITY! You are missing out on the newest capabilities and enhanced security. For information on all the latest features, see the CIMPLICITY product page. For more information on upgrades, contact your GE Digital sales agent or e-mail GE Digital Sales Support. For the most up-to-date documentation, go here.
Enter one: Command path name, folder name, document name with a registered extension, web page reference. Click browse to open the Windows Select a Command dialog box.
Note: If the path name contains spaces, enclose it in double quotes.
3
Arguments
(Usually blank) Addition information used by the program
Opens a Text Box to enter arguments.
4
Working directory
Directory path to command if it is different from the screen file directory.
Opens a Browser for Folder browser.
5
Run minimized
When checked, minimizes window associated with the command.
6
Confirmed
When checked, Confirmed requires confirmation at runtime.
A message box will display before the action occurs requesting confirmation to proceed.
Default
Clear
Confirmation is not required.
7
Message
Opens a Text Box to enter a customized confirmation message.
8
Translate message
Check to make the customized message text available to be emitted to the selected translation file.