Terminal Server Setup
Procedure
-
Log into your terminal server, and set privileged mode by issuing the following command. Enter the privileged password when prompted (typically "system"):
> set priv
Password>
-
Enter the following command so that the permanent database and the operational database will be updated when a define command is issued:
>> set server change enabled
-
For each port to which a marquee is attached, enter the following set of commands where:
<port> is the actual port number to which the marquee is attached. Note that it is possible to specify a range of port numbers instead of a single port (for example, 1-10 signifies ports 1 through 10).
<ip_port> is the telnet port number.
<parity> is odd, even, or none.
<stop bits> is the number of stop bits.
<speed> is the baud rate of the marquee.
>> define port <port> access remote >> define port <port> telnet remote <ip_port> >> define port <port> telnet transmit immediate >> define port <port> parity <parity> >> define port <port> character size 8 >> define port <port> stop bits <stop bits> >> define port <port> autobaud disabled >> define port <port> speed <speed> >> define port <port> line editor disabled >> define port <port> telnet csi escape enabled >> define port <port> telnet binary session mode passall >> define port <port> loss notification disabled >> define port <port> autoprompt disabled >> define port <port> verification disabled >> define port <port> outboundsecurity disabled >> define port <port> broadcast disabled >> define port <port> default session mode transparent >> define port <port> internet tcp keepalive 2