MOC Administration
Management of Change: MoC Administration
This workflow describes the process for creating Exceptions, Answer Options, Questions, and Checklists that can be used in a Change Project.
In the following workflow diagram, the blue text in a shape indicates that a corresponding description has been provided in the sections that follow the diagram. For more information, refer to the topic Interpreting the Workflow Diagrams.

Create Exceptions
Persona: Solution Administrator
Create the Exceptions that represent the action items that will be created automatically when you select Answer Options in a Checklist in a Change Project.
Create Answer Options
Persona: Solution Administrator
Create additional Answer Options that you want to use when you create Questions.
Create Questions
Persona: Solution Administrator
Create the Questions that you can want to associate with Checklists. You must associate each Question with a minimum of two Answer Options. As needed, you can associate an Answer Option with an Exception.
Create Checklists
Persona: Solution Administrator
Create Checklists by adding Questions as Checklist Items to each Checklist.
Change Project
Persona: Analyst
Go to the Change Project workflow.