GE Digital APM Database Server
Hardware Requirements
The following hardware requirements outline the minimum hardware required for any machine that will serve as the GE Digital APM Database Server. These requirements account for the GE Digital APM software only. Additional hardware may be required on GE Digital APM Database Server machines where components other than the GE Digital APM database are installed. These requirements may not be sufficient, depending upon how your system is configured.
Component | Requirement |
---|---|
Core | Eight Processor Cores, 2+ GHz |
RAM | 32 GB RAM |
Hard Drive | 200 GB of available hard drive space on, at a minimum, 10K RPM drives |
-
While GE Digital APM supports the use of RAID 5, which has benefits in its recoverability features, GE Digital APM recommends the use of RAID 10 for the best overall database performance.
-
Oracle requires instance tuning to use memory cache effectively. For Oracle Database Servers, a comparable UNIX-based system can be used.
-
A minimum of a 100BASE-TX switched network is required between the GE Digital APM Server and the GE Digital APM Database Server.
Software Requirements
GE Digital APM supports the use of an Oracle or SQL Server Database Server.
Oracle Requirements
The GE Digital APM testing environment includes Oracle Server 12.1.0.1, 12.1.0.2, 12.2.0.1.0, and 12.2.0.3 (19c).
SQL Server Requirements
GE Digital APM requires that you use SQL Server 2016, SQL Server 2017, or SQL Server 2019. The GE Digital APM testing environment includes SQL Server 2016 SP1, SQL Server 2017 RTM, and SQL Server 2019 RTM.