SIS Trip Reporting
SIS Management: Trip Reporting Workflow
This workflow describes the process of saving and analyzing trip reports.
In the following workflow diagram, the blue text in a shape indicates that a corresponding description has been provided in the sections that follow the diagram. For more information, refer to the topic Interpreting the Workflow Diagrams.

Create Trip Report
Persona: Analyst
Create a Trip Report record to store the details of the trip that occurred.
Select Logic Solver
Persona: Analyst
Select the Logic Solver that is associated with the Instrumented Functions for which the trip occurred.
Select Applicable Instrumented Functions
Persona: Analyst
Select the Instrumented Functions that are associated with the trip that occurred.
Is Trip As Designed?
Persona: Analyst
Determine whether the trip was as designed, spurious, or dangerous.
Record Details of Failed Component
Persona: Analyst
If the trip was not as designed (i.e., spurious or dangerous), then enter the details of the Protective Instrument Loop element that caused the trip. For example, if a trip was caused when a sensor indicated high pressure even when the pressure level was normal, enter the details of the sensor. For that example, the trip type would be Spurious.