Inspection Configuration
Access the Inspection Configuration Workspace
Procedure

About Checklist Configuration Templates
Checklist Configuration Templates allow you to define a collection of checklist categories and the items that they contain to create Checklist Templates. Users can create Inspection Events using the Checklist Templates, and the Checklist Finding records are generated based on the selected template.
Using Checklist Configuration Templates
Checklist Configuration Templates should contain checklist categories and items that will result in detailed Checklist Templates that can be used to create Inspection Events. In the Checklist Configuration Templates section, you can create Checklist Configuration Templates that contain multiple checklist categories and items that are defined based on system code tables. You can modify the available checklist categories and items using the MI CHECKLIST CATEGORIES system code table. When you add a category to a Checklist Configuration Template, you can choose which items appear in the checklist. You can continue adding checklist categories and items to your Checklist Configuration Template until you have created a Checklist Template that will be useful for the intended asset. Creating a Checklist Configuration Template with checklist categories and items that correspond closely to existing assets streamlines inspections by including relevant Checklist Finding items in a user-created Inspection Event.
Checklist Configuration Templates and Taxonomy Configuration
The Checklist Configuration Templates that you create can be linked to a Taxonomy Configuration. When a Checklist Configuration Template has been linked to a Taxonomy Configuration, the Checklist Template appears as an option when users create Inspection Events for an asset whose equipment taxonomy matches the Taxonomy Configuration. The Checklist Configuration Template will also appear by default if the equipment taxonomy of the asset does not match an existing Taxonomy Configuration.
Checklist Configuration Templates and Asset Mapping
Asset Mapping allows the Checklist Template categories to be associated with the existing Assets. When creating or editing a Checklist Configuration Template, the Enable Asset Mapping option is available in the Template Name window. If you select this option when creating an Inspection Event using the Checklist Configuration Template, an Asset Mapping section appears, allowing you to map the Assets to the checklist categories.
Example: Fire Tube Boiler
A Checklist Configuration Template named Fire Tube Boilers Inspection Checklist contains the Tubes Waterside checklist category. The Tubes Waterside checklist category contains two items: Borescope Inspection and Corrosion.
When a user creates an Inspection Event, a Checklist Template named Fire Tube Boilers Inspection Checklist appears in the Inspection Event list. If the user creates an Inspection Event using the Fire Tube Boilers Inspection Checklist Checklist Template, the Checklist Finding record displays the Tubes Waterside checklist category with Borescope Inspection and Corrosion listed as Checklist Finding items.
Example: Fire Tube Boiler linked to a Taxonomy Configuration
The Fire Tube Boilers Inspection Checklist is linked to the following Taxonomy Configuration:
- Taxonomy Category: Fixed
- Taxonomy Class: Boiler
- Taxonomy Type: Misc Boiler
When a user creates an Inspection Event for an asset that shares that Taxonomy Configuration, Fire Tube Boilers Inspection Checklist appears in the list of available Checklist Templates for that asset.
About Application Configuration
This topic has been intentionally excluded from the APM product documentation website. This topic is available to you via the product documentation that is provided within the APM system.
Configure Status to State Mapping
About This Task
APM supports uses of both Status and State Management for the approval work process of Inspection Recommendation. If you are currently using the Status field in Inspection Recommendation for the approval work process and want to use the State Management for Inspection Recommendation, you must map each Status value in the Inspection Recommendation Status field to a corresponding State in Inspection Recommendation State Configuration. After you configure and save the mapping, you must upgrade the existing Inspection Recommendation records using the Upgrade Records button so that all the Status values are updated to the mapped States. This ensures that current approval work process for Inspection Recommendation now uses states.
For example, the following Inspection Recommendation records are using the Status field.
Recommendation ID | Asset ID | Functional Location ID | Recommendation Headline | Status |
---|---|---|---|---|
REC-21 | HE-1608 CRUDE-HVY. ATMOS. GAS OIL | 016-E-E3104A CRUDE-HVY. ATMOS. GAS OIL | Shell Corrosion | Created |
Rec-2005 | HE-1608 CRUDE-HVY. ATMOS. GAS OIL | C-488 LUBE/SEAL OIL COOLER ~ HXST 105 | General Corrosion | Pending Review |
Rec-244 | HE-1608 CRUDE-HVY. ATMOS. GAS OIL | C-488 LUBE/SEAL OIL COOLER ~ HXST 105 | General Distortion | Pending Review |
Source Family | Status | State |
---|---|---|
Inspection Recommendation | Created | Proposed |
Inspection Recommendation | Pending Review | Pending Approval |
Recommendation ID | Asset ID | Functional Location ID | Recommendation Headline | State |
---|---|---|---|---|
REC-21 | HE-1608 CRUDE-HVY. ATMOS. GAS OIL | 016-E-E3104A CRUDE-HVY. ATMOS. GAS OIL | Shell Corrosion | Proposed |
Rec-2005 | HE-1608 CRUDE-HVY. ATMOS. GAS OIL | C-488 LUBE/SEAL OIL COOLER ~ HXST 105 | General Corrosion | Pending Approval |
Rec-244 | HE-1608 CRUDE-HVY. ATMOS. GAS OIL | C-488 LUBE/SEAL OIL COOLER ~ HXST 105 | General Distortion | Pending Approval |
Currently, APM only allows mapping of Status to States. After you upgrade the Inspection Recommendation records using this feature, you can switch back to Status by clearing the Use State Management for Inspection Recommendation check box. However, the existing Inspection Recommendation records cannot be reverted to Status. To align Inspection Recommendations with other performance recommendations, we recommend using State Management to manage Inspection Recommendations.
Before You Begin
- Make sure that the State Functionality is enabled in the State Configuration section of the Inspection Recommendation Family Management.
- Make sure that the Inspection Admin role or the Super User role is assigned to you.
Procedure
About Event Configurations
This topic has been intentionally excluded from the APM product documentation website. This topic is available to you via the product documentation that is provided within the APM system.
Modify the Asset Query Path and the Alerts Query Path
About This Task
The Asset Query Path and the Alerts Query Path fields are populated with default query paths. This topic describes how to modify these values.
Procedure
Modify Profile Configuration
Procedure
- Modify the Taxonomy Profile Configuration
- Modify the Profile System Code Configuration
- Modify the Profile Query Configuration
- Modify the Profile Query Configuration
Results
Delete a Taxonomy Profile Configuration
Procedure
Modify Method Configuration
Procedure
- Modify the Method System Code Configuration
- Modify the Method Query Configuration
Add or Modify Event Configuration
Procedure
- Add an Event Configuration
- Steps: Modify an Event Configuration
Modify or Delete Family Preferences
Procedure
- Modify Related Family Preferences
- Delete a Related Family
- Steps: Delete a Related Family
- Delete a Related Family
- Delete a Related Family
Delete an Event Configuration
Procedure
Access a Checklist Configuration Template
About This Task
Super Users and members of the MI Inspection Security Group who also have an Inspection Administrator resource role can use the Inspection Configuration workspace to configure the information that is displayed in Inspection Management. For more information, see the documentation for Inspection Management.
Procedure
Create a Checklist Configuration Template
Procedure
Delete a Checklist Configuration Template
Procedure
Add Categories and Items to a Checklist Configuration Template
About This Task
After creating a Checklist Configuration Template, you can select a checklist category from which you want to add items to the template. The selected checklist category is used to sort your selected items in the template. You can add multiple checklist categories that each contain one or more items to your Checklist Configuration Template.