FMEA Analyses
About FMEA
A Reliability Centered Maintenance (RCM) analysis evaluates a system with respect to its individual function to determine how to avoid functional failures. Failure Modes and Effects Analysis (FMEA) focuses on actual equipment and locations, and analyzes how each piece of equipment or location can fail and the effect of each failure. In other words, an RCM Analysis is conducted for the purpose of maintaining the function of a system. An FMEA Analysis is conducted for the purpose of maintaining the system itself.
Specifically, FMEA is a method used to identify the potential failures of equipment and locations, describing the possible effect of each failure, and implementing recommended actions for actions that can be taken to prevent the failures from occurring.
Access an Analysis
Procedure
Create a New FMEA Analysis
About This Task
Procedure
Create an Analysis from a Template
Procedure
Apply Asset Template on Analysis
Procedure
Modify an FMEA Analysis
About This Task
Procedure
Copy and Paste Nodes in an Analysis or Template
Procedure
Promote an FMEA Analysis to Strategy
About This Task
Promoting an FMEA analysis to an ASM strategy creates risks and actions in a new strategy from corresponding failure effects and Recommended Actions in an FMEA analysis, respectively. Additionally, when you make subsequent changes to the original FMEA analysis, you can also promote those changes to the strategy.
Procedure
Export an FMEA Analysis
Procedure
Results
- You can also export an analysis from the Analysis Details workspace by selecting
, and then selecting Export.
- All Secondary Actions associated with the FMEA analysis are also exported.
Use State Controls in FMEA Analyses
About This Task
Procedure
Delete an FMEA Analysis
About This Task
Procedure
Access a Reference Document
Procedure
Link Reference Documents
Before You Begin
This topic assumes that there are existing documents in FMEA that you want to link to your analysis.
Procedure
Delete a Reference Document
Before You Begin
Procedure
Access an Asset
Procedure
Filter FMEA Analyses by Asset
About This Task
APM features asset-centric navigation. To filter strategies by asset, please follow the instructions below.
Procedure
Link an Asset to an Analysis
Before You Begin
Procedure
Delete an Asset
Before You Begin
Procedure
Use the Decision Logic Builder in FMEA Failure Effects
Before You Begin
- The Decision Logic Builder guides you step-by-step through answering questions that will result in suggestions for mitigating a given failure effect. After you use the Decision Logic Builder to determine which actions should be taken to mitigate the effects of the failure, you can create Recommended Actions.
- The Decision Logic Builder will pose a series of Yes or No questions. When you complete all steps in the Decision Logic Builder, you will be presented with a recommended action that is based on your responses. You can then view a summary of your responses on the Decision Logic tab of the failure effect.
- The Decision Logic Builder is based upon the concepts and decision diagrams in SAE Standard JA1012, "A Guide to the Reliability-Centered Maintenance (RCM) Standard." The process and terminology used in the Decision Logic Builder are described in more detail in this standards document. To use the Decision Logic Builder effectively, you will need to be familiar with this standard.
- This topic assumes that you have a pre-established FMEA analysis with failure modes.