General Reference
APM Connect Version Compatibility Table
This topic provides the installation files that are required for an APM Connect installation, and the version structure for APM Connect.
Version Structure
Example: | EAM | SAP | V1 | 5 | 2 |
---|---|---|---|---|---|
Description: | Area of APM Connect (that is, Data Loaders, EAM, M2M) | EAM System released against (that is, SAP, SAP PI, Maximo) | Architecture Release | Major Release | Maintenance or Patch Release |
The following are examples of how to interpret the versions.
- EAM SAP V1.5.0 is the fifth major release on the APM Connect V1.x architecture; it can be applied to the EAM system SAP.
- EAM SAP V1.5.1 is a maintenance release that can be applied to EAM SAP V1.5.0.
- DL V1.4.0 is the fourth major release on the APM Connect V1.x architecture.
APM Compatibility Table
This table includes only the APM versions for which a corresponding APM Connect version was released.
APM Framework Version | APM Connect Base | Integrated Pack Version | SAP ABAP Version |
---|---|---|---|
V4.6.x | APM Connect Services V5.1.2.0.0 | Integration Pack (IP-Release_5_1_2) | V7.X |
V4.5.0.0.0 | APM Connect Base V2.0.0 | UDLP Version: UDLP V2.9.0 or V2.8.0 or v2.9.0.1 (with ABAP V7.X) | V4.X |
SAP Certificate Number | Certificate Issue Date | Certificate Expiration Date | SAP Version | ABAP Interface Version (as displayed on the certificate) | APM Versions |
---|---|---|---|---|---|
16649 | June 26, 2020 | June 25, 2023 | S4/HANA 1909 | V4.X | 4.4.x, 4.5.x, 4.6.x, (UDLP 3.3.0) |
13857 | October 6, 2020 | October 5, 2023 | ERP (ECC) 6 EHP8 | V7.X | 4.6.x, 5.x |
16864 | January 21, 2021 | January 20, 2024 | S4/HANA Cloud Extended Edition 1909 | V7.X | 4.5.x*, 4.6.x, 5.x |
17051 | January 21, 2021 | January 20, 2024 | S4/HANA 1909 | V7.X | 4.5.x*, 4.6.x, 5.x |
17336 | January 21, 2021 | January 20, 2024 | S4/HANA Cloud Extended Edition 2020 | V7.X | 4.5.x*, 4.6.x, 5.x |
17337 | January 21, 2021 | January 20, 2024 | S4/HANA 2020 | V7.X | 4.5.x*, 4.6.x, 5.x |
20873 | October 12, 2022 | October 11, 2025 | S4/HANA Cloud Extended Edition 2021 | V7.X | 4.5.x*, 4.6.x, 5.x |
20874 | October 12, 2022 | October 11, 2025 | S4/HANA 2021 | V7.X | 4.5.x*, 4.6.x, 5.x |
21395 | July 20, 2023 | July 20, 2026 | S4/HANA 2022 | V7.X | 4.5.x*, 4.6.x, 5.x |
24053, 24054 | Nov 05, 2024 | Nov 05, 2027 | S4/HANA 2023 | V7.X | 4.6.x, 5.x |
The Automatic Data Loader Directories
The automatic data loader job uses directories within the directory identified in the SCAN_DIR parameter to identify the data loader to use for a particular workbook.
Data Loaders and Directories
Data Loader Name | Directory Name |
---|---|
APM Family | ManageAPM |
Asset Criticality Analysis (ACA) | ACADataLoader |
Asset Criticality Analysis (ACA Checklist) | ACACheckListDataLoader |
Asset Ingestion Loader | AssetIngestionLoader |
Asset Strategy Management (ASM) | ManageASM |
Asset Strategy Management (ASM) Templates | ManageAssetStrategyTemplate |
Calibration | Calibration Loader |
Custom Asset Hierarchy | Custom Asset Hierarchy Loader |
Equipment and Functional Location | ManageEquipmentAndFunctionalLocation |
Failure Modes and Effects Analysis (FMEA) | ManageRCMFMEA |
Failure Modes and Effects Analysis (FMEA) Analysis Templates | ManageFMEAAnalysisTemplate |
Failure Modes and Effects Analysis (FMEA) Asset Templates | ManageFMEAAssetTemplate |
Generation Availability Analysis (GAA) Amplification Codes | GAA GADS Amplification Code |
Generation Availability Analysis (GAA) Cause Code | GAA GADS Cause Code |
Generation Availability Analysis (GAA) Events | GAA Events |
GAA Wind Asset Hierarchy | GAA Wind Asset Hierarchy |
GAA Wind Events | GAA Wind Events |
GAA Wind Sub Group Capacity | GAA Wind Sub Group Capacity |
Geographic Information System (GIS) | GISDataLoader |
Hazards | Hazards Loader |
Inspection Management (IM) Assets | ManageInspections |
Inspection Management (IM) Functional Location | ManageInspectionsFL |
Production Loss Analysis (PLA) Admin | PLA Admin Data |
Production Loss Analysis (PLA) Plan | PLA Plan Data |
Production Loss Analysis (PLA) Production Event | Production Event Data |
Reliability Centered Maintenance (RCM) | ManageRCM |
RCM Analysis Template | ManageRCMAnalysisTemplate |
Risk Based Inspection (RBI) 580 | ManageRBI580 |
Risk Based Inspection (RBI) 581 | ManageRBI581 |
Risk Based Inspection (RBI) Corrosion Loop | Load RBI Corrosion Loop |
Risk Matrix | RiskMatrixDataLoader |
Role | RoleDataLoader |
Root Cause Analysis (RCA) | Manage RCA |
Rounds Allowable Values | Rounds Allowable Value |
Rounds Readings | Rounds Readings |
Rounds Routes | Rounds Route |
Rounds Templates | Rounds MLTG |
Tags to Assets Relationship | ManageTagLinks |
Taxonomy | ManageTaxonomy |
Thickness Monitoring (TM) Equipment | ManageTMLGroup |
Thickness Monitoring (TM) Functional Location | ManageTMLGroupFL |
Work History | ManageWorkHistory |
About Time Zone Data
APM stores the dates and times of transactions in Universal Coordinated Time (UTC) format. This enables the data to flow through the system in a single time zone format. APM Connect supports the time zones defined in https://docs.microsoft.com/en-us/previous-versions/windows/embedded/gg154758(v=winembedded.80).
To provide information with the time stamp relevant to your operations, the system converts UTC to your time zone by using the time zone information configured in your user definition.
The following sections contain the time zone considerations relevant to specific systems.
Maximo
APM stores the time stamp associated with the data extracted from Maximo in UTC and displays the time stamp based on your configured time zone.
SAP
SAP provides a set of baseline time zone codes, which contain most of the standard time zones across the world. SAP also provides the ability for administrators to define their own custom time zone, as needed. Before you use a customized time zone, you must configure the timezone_control table in APM Connect to include the customized time zone.
SAP defines two types of time zones:
- System: This time zone is based on SAP Application Server Operating System and is derived from the context file. You cannot modify this type of time zone.
- User: This time zone is based on the user who created the SAP record. You can modify and store this type of time zone in the SAP user interface.
APM stores the time stamp associated with the data extracted from SAP in UTC and displays the time stamp based on the time zone configured for the user who created the SAP record.
Support for Multiple Source Systems
Whether in a cloud environment or an on-premise installation, APM Connect enables you to connect multiple source systems to a single APM system.
There are occasions when you need to connect multiple source systems to a single APM system. For example, when your company acquires another company, rather than immediately attempting to merge two systems together, you need to keep the systems running separately but want to implement strategies centrally. The two systems might be the same type or of different types. You can configure APM Connect to handle either scenario.
The steps to configure these scenarios is similar to configuring a single system; you repeat the steps that define the EAM system records and, after creating the intermediate repository for the first system, run a job that adds the other systems to the intermediate repository with any required extraction filters.
Multiple Source Systems of the Same Type
This scenario is most useful when you all systems you need to support are the same type. The context file configuration for each source system will look the same for the target APM and APM Connect system for all the source systems. The unique parts of the context file are those that describe the particulars of the source system, for example, the system ID and filters used.
Multiple Source Systems of Different Types
Use this scenario if you need to support multiple disparate systems, for example, an SAP and a Maximo system. In this case, you will need to configure context files for each different type of source system, each pointing to the same target APM and APM Connect system. This does not preclude having multiple systems of a specific type (for example, one SAP, one ServiceMax, and two Maximo).
Considerations
There are some things to consider when connecting multiple source systems to a single APM with APM Connect:
- You must make sure that each source system has a unique system ID.
- The logs will contain the messages from all of the source systems. Each message will identify the source system using the system ID.
- Some source system types have unique requirements that must be performed for each source system. For example, you must run the Static Data job for all SAP systems.
- Each source system in a cloud environment will need an intermediate repository, even though they are communicating with a single tenant.
- Do not schedule running the same adapter job types (for example, functional location extractions) simultaneously from different source systems.
Support for Multiple Culture Settings from a Single Source System
APM Connect enables you to send data to APM from a single source system that supports plants using different language or extraction requirements.
Globalization has increased the need to improve management of assets in different culture settings. Your solution may involve including these new plants in a single source system that communicates with APM but requires the data to be presented to the user in their native language. You can accomplish this by configuring APM Connect so that the plants that require specific languages or extractions appear to be different source systems, one for each language or extraction requirement. This capability provides a better user experience for all users of APM regardless of their location.
A key advantage of this support is that you can combine your source systems and then configure APM Connect to extract the data correctly.
Considerations
- The user defined in the source system that communicates with APM must use the same decimal notation.
- You must have unique system IDs and the correct language parameter value or extraction requirements for each plant.
- You must configure filters to make sure that the data is routed correctly to the specific location.