Overview
Overview of the Rounds Pro Module
In industrial sectors with plant-based organizations, enterprise assets and equipment are monitored by operators at regular intervals at multiple points to ensure health and safety. The Rounds Pro module provides enhanced features to monitor the health of the assets in a plant and detect technical problems and failures with ease, thus improving the performance of assets in the plant.
Using the Rounds Pro, operators in a plant can perform inspections proactively by identifying issues and initiating preventive or remedial actions. Rounds Pro serves as a data connect between the assets in a plant and the APM database, which helps to drive preventive and predictive maintenance of the plant.
Using Rounds Pro and the Rounds Pro mobile app, installed on hand-held devices, the operator can perform the day-to-day management of tasks through routes, steps, built-in reporting, and data collection. The module helps to identify irregularities in the assets based on the data collected and enables the operators to take corrective actions.
Access the Rounds Pro Manager Page
Before You Begin
You can access the Rounds Pro Manager module from the left navigation menu under the Health option only if you are a member of the MI Rounds-Pro Admin Security Role.
You can perform various tasks on this page based on the privileges granted to the Security Groups associated to the MI Rounds-Pro Admin Security Role.
Procedure
- Route Masters: Displays a list of available routes in the database with a brief description and the status of the routes.
- Open Instances: Displays the list of open route instances that have been created from the Route Masters.
- Instance History: Displays history of route instances that have been checked in or completed.
- Steps: Displays a list of steps that are used to monitor assets for specific Measurement Locations.
- If APM is deployed on an on-prem environment, and you select the Open Dashboard link, the on-prem dashboard is displayed.
- If APM is deployed on a unified environment, and you select the Open Dashboard link, the IBI dashboard is displayed.
- COMPLIANCE OVERVIEW: This chart displays the percentage of routes that are due in the next 30 days, due in the next week, due today, and overdue.
- YEAR TO DATE COMPLIANCE: This chart displays the number of route instances that are completed from the beginning of the year till date.
- NON-COMPLIANT ROUTES: This graph displays the number of route instances that are non-compliant for different route masters. When you select a route master, the graph provides the details about the assignment of each route instance.
Access the Rounds Designer Page
Procedure
Rounds Pro Workflow
This workflow provides the basic, high-level steps for using Rounds Pro. The steps in this workflow do not necessarily reference every possible procedure.
- In Rounds Pro, select an asset and create a Step.
- Create the Picklists, health indicators, and conditions for the Step.
- Create a Route by adding Steps. Save the Route to the Route Masters.
- Create a Route Instance using the web application.
- Access the Open Instances in My Routes using the Rounds Pro mobile app.
- Execute the route.