Rounds Reports

About Rounds Reports

In the Rounds Designer module, you can generate reports detailing either the Measurement Locations or Lubrication Requirements on a specific Route. You can also narrow the scope of these reports so that they contain information on only Checkpoints that are overdue or Measurement Locations whose last reading value triggered an alert. You can save these reports in a variety of file formats and print them so that you can record reading values at the associated Checkpoints.

Access the Reports Section

About This Task

You can use the Reports section to access the reports stored in the Rounds Catalog folders and view them in the Report Viewer.

Procedure

  1. Access the RD Overview page.
  2. In the RD Overview page, select the Reports tab.

    The Reports section appears.



    The Reports section displays one row for each report stored in the Rounds report folders. The section contains the button, which allows you to search for reports that are stored in the database. The section also contains the following columns:

    • Report Caption: Displays the report captions as hyperlinks, which you can select to access the report.
    • Description: Displays the report description.

Access a Report from the Reports Section

Procedure

  1. Access the Reports section.
  2. In the grid, select the hyperlinked caption of the report that you want to access.
    Note: If the report is based on a query that contains prompts, the Enter Query Parameters dialog box will appear. After you select the desired values, select OK to view the report.

    The selected report appears in a new page, in which you can perform various tasks.