Overview

Overview of the Production Loss Analysis (PLA) Module

Using the APM Production Loss Analysis (PLA) module, you can compare the actual production with the planned production, and thus uncover any minor or major factors that cause production losses.

In addition, you can:

  • Enter the production data.
  • Identify production losses and associate them with the events that caused them.
  • Determine what types or categories of events cause your company to lose production.

By entering and evaluating production data, you can easily identify ways in which you can reduce unplanned downtime and increase production in the future, thus reducing cost and increasing profit.

More Details

The following graph represents a company's optimal, planned, and actual production percentage for a year.

In the graph, the blue line indicates that the maximum demonstrated rate or the percentage of output the company can produce during the optimal operating conditions is 100%.

The yellow area displays the planned production percentage for each month. Because the managers know that they cannot produce 100% of this maximum output each month, the planned production rate is lower than 100% during some months. In March, the planned production rate is 0% because the company shut down its units to perform maintenance, install new equipments, and so on.

The red bars indicate the actual production rate each month. For some months, the company produced the amount that they had planned, whereas for others, they produced less than they had planned.

Thus, you can conclude that more than half of the production losses for the year was due to the shutdown in March. If they could find a way to reduce this shutdown time or eliminate it completely, the overall production would increase.

Using PLA, you can also determine exactly how much money your company lost during the shutdown in March and during the months when they could not reach the 100% production rate. You could then categorize these losses into planned and unplanned losses.

Access the PLA Overview Page

About This Task

This topic describes how to access the PLA Overview page, on which you can view all the information and perform tasks related to the production of various hierarchy levels.

You can perform the various tasks on this page based on the Security Groups to which you are assigned.
Tip: For more information, refer to the Security Group topic for this module.

Procedure

In the module navigation menu, select Reliability > Production Loss Analysis.

The PLA Overview page appears.

The tabs at the top of the page summarize the number of items in each category. You can select a tab to view one of the following lists:

  • Production Data: Contains a list of Production Plans that contain incomplete Production Data.

    Note: The number on the Production Data tab only includes Production Plans that are in progress. Production Losses do not have to be reconciled for Production Data to be considered complete.
  • Production Plans: Contains a list of all Production Plans available in the APM database.
  • Production Events: Contains a list of Production Events available in the APM database and allows you to create new Production Events.
  • Production Analyses: Contains a list of Production Analyses, which are created in the PLA module.

On the page, you can also view the following sections:

  • Planned Production vs Losses : Plots the planned production, actual production, and losses for given time period. By default, this chart shows values for last 90 days. You can select on the upper-left corner of the PLA Overview page to modify the time period to 120 days or 365 days.

    In the chart:

    • The line representing Actual shows the number of units that were produced for a specific month. The horizontal axis (X) represents months. You can select a datapoint to view the total number of units produced in that month.
    • The bars representing Short Range Plans show the number of units that were planned to be produced for the specific month. You can select a bar to view the total number of units planned to be produced in a month and number of the month for which you are viewing the planned production.
    • The bars representing Losses show the amount of production (in number of units) that was lost. You can select a bar to view the total losses for a month and number of the month for which you are viewing the losses.

    While viewing the chart, you can select in the upper-right corner of the chart to modify the appearance of the plot using standard graph features.

  • Top 10 Bad Actors: Contains a chart that plots the total cost of losses that were contributed by the top 10 bad actors within a selected hierarchy level for a given time period. The losses represented here are the total amount of production lost for the affected plans, products, and units. By default, this chart shows values for last 90 days. You can select on the upper-left corner of the PLA Overview page to modify the time period to 120 days or 365 days.
  • Event Summary: Contains a chart that plots the count of Production Events filtered by the Event Code percentage for a given time period. By default, this chart shows values for last 90 days. You can select on the upper-left corner of the PLA Overview page to modify the time period to 120 days or 365 days. You can select a datapoint for a Production Event to view:
    • The Event Code
    • The count of each Event Code
By default, the hierarchy level is set to Home. You can select on the upper-left corner of the page to filter the hierarchy level. The Production Loss Analysis information on the page is related to an Asset by default. If you also want to include Production Loss Analysis information that is not related to an Asset, in the Include analyses without any assets? box, select Yes. You can specify the time period for the graphs on the PLA Overview page by selecting the time period from the Period list, as needed.

PLA Workflow

This workflow provides the basic, high-level steps for using PLA. The steps and links in this workflow do not necessarily reference every possible procedure.

  1. For each production unit, create a production plan to specify the amount of product you plan to produce during a set time period. You can create the plan on any schedule, such as yearly, quarterly, monthly, and so on.
  2. If an event such as an equipment failure or a planned shutdown occurs and causes you to incur a production loss, document the event.
  3. Enter production data on a daily basis. This includes entering the amount of product that you produced and accounting for any losses that you incurred each day.