Checklists
About Checklists
In the Application Settings for MOC, you can create Checklists for various purposes. For example, you can create a checklist for temporary changes, a checklist for permanent changes, a checklist for planning, a checklist for post implementation assessment, and so on. In the Change Project, based on your needs, you can add one or more of Checklists to the project. Checklists created in the Application Settings are used as a template when you add them to the Change Project.
When you add a Checklist to a Change Project, APM creates copies of the Checklist and the associated Questions and Answer Options. The Change Project is then associated with the copy of the Checklist. This ensures that any changes to the original Checklist do not affect the Change Project.
Access a Checklist
About This Task
This topic describes how to access a Checklist that is associated with a Change Project. You can also access a Checklist that you created using the Application Settings for MOC.
Procedure
Add a Checklist to a Change Project
Before You Begin
Procedure
Results
- Copies of the Questions and Answer Options associated with the selected Checklist are created, and then associated with the copy of the Checklist.
- Copies of the Exceptions associated with Answer Options are also created.
What To Do Next
Respond to Questions in a Checklist
Procedure
Results
- For each Question, if the selected Answer Option is associated with an Exception, then an association is created between the Exception and the Change Project. The Exception appears in the Exceptions and Tasks workspace.
What To Do Next
Modify Response to a Question in a Checklist
Procedure
Results
- Any association between an Exception, created as a result of the previously selected Answer Option, and the Change Project is removed. The Exception and the associated Tasks do not appear in the Exceptions and Tasks workspace.
-
If the Answer Option you selected in step 2 is associated with an Exception, then an association is created between the Exception and the Change Project. The Exception appears in the Exceptions and Tasks workspace.
What To Do Next
- If an Exception has been associated with the Change Project, then create Tasks for the Exception.