Overview
About Manage Translations Page Tasks
You can use the Manage Translations page to manage all the translatable strings that are displayed throughout APM for all Security Users whose APM Culture setting corresponds to a set of installed translation files. You can access this page from the Configuration Manager.
- Download the following types of translations to a Microsoft Excel file, which you can use to review and customize the translations:
- Export your untranslated metadata strings to a Microsoft Excel file, which you can use to provide translations for those strings.
- Upload the following types of translations to APM:
- Delete the following types of translation files:
- Custom metadata string translation files.
-
Custom application string translation filesNote: You cannot delete baseline translation files.
Any changes that you make to a translation file using this tool will be applied wherever the affected translation is used.
- Metadata : Provides options that you can use to manage metadata string translations.
- Application : Provides options that you can use to manage application string translations.
About the Microsoft Excel File for Translations
Metadata string and application string translations are stored in APM as MTM files. You can download the translations to your local machine, where they will be converted to Microsoft Excel files so that you can work with the translations. After you are finished, you can upload the Microsoft Excel file, and the APM system will create or update the MTM files stored in the APM as needed.
The name of each Microsoft Excel file appears as <Language>.xlsx, where, <Language> is the language into which the application or metadata content is translated.
- Word: The default string. This is the string whose translation you can manage in that row.
- Translated Word: The translation for the string that appears in the Word cell in that row. This is the only value that you should modify in the Microsoft Excel file. Before you customize a translation, you should know how to work with translations in the Microsoft Excel file.
- Name: This value is used by APM system.
- Path: This value is used by APM system.
- Accessed: This value is used by APM system.
- Fit: This column is not used.
About Working with Translations in the Microsoft Excel Files
When you open a Microsoft Excel file containing translations for a language, you should modify only the strings that are stored in the Translated Word column. Before you do so, you should review the following guidelines:
- If a string includes {0}, {1}, {2}, and so on, you should not modify the numeric value or remove the brackets { }. These values are used by APM system.
- If a string includes an ampersand (&), such as (&S), you should not remove the & symbol, change the letter of the alphabet that appears beside the & symbol, or remove the parentheses that appear around the & symbol and the letter of the alphabet. These values are used by APM system.
- If a string includes special characters such as a colon (:) or ellipsis (...), you should not remove these characters. These characters are used by APM system.
About the APM Culture Setting
The APM Culture setting is the value in the Culture drop-down list box in APM Security User records. The APM system uses this setting to determine which translation files to use when a user logs in to a APM. For example, if the APM Culture setting of a user is Spanish (Spain), that user will see Spanish translations throughout APM.
Before a user can see the translated strings in APM, their Security User record must contain a corresponding Culture setting.
The following table provides a mapping from each APM Culture settings to the translations that are currently available in APM. We recommend that you use this list as a guide for configuring APM Security User records.
Non-English Version of APM | APM Culture Setting(s) |
---|---|
Chinese |
Chinese (People's Republic of China) -or- Chinese (Simplified) |
Dutch | Dutch |
French | French (France) |
German | German |
Italian | Italian (Italy) |
Portuguese | Portuguese (Brazil) |
Russian |
Russian -or- Russian (Russia) |
Spanish | Spanish (Spain) |
Japanese Note: Japanese is not currently available for Rounds Data Collection on Windows mobile devices. |
Japanese -or- Japanese (Japan) |
Polish | Polish (Poland) |
About the Translation Files
- One file stores the baseline translations for application strings.
- One file stores the baseline translations for metadata strings.
The translation files are named according to the abbreviation for the culture associated with the language that is stored in that file. For example, the Spanish translation file is named es.MTM, where es is the abbreviation for Spanish.
If you customize baseline translations or add new translations, custom translation files will be created automatically to store those translations. For example, suppose that for Spanish, you want to modify the translation for the baseline string Equipment. Suppose that the same string Equipment appears both as a button label (application string) and as a datasheet caption (metadata string).
To modify a translation, you can download to your local machine the translations stored in the appropriate translation file from the APM. These translations will be downloaded to a Microsoft Excel file, which you can use to modify the translations. After you modify the translation strings, you can upload the Microsoft Excel file, and the APM system will automatically convert that file to a translation file (that is, with the extension MTM) and save it.
The APM system will display only the strings that are stored in translation files in APM. If you have uploaded custom translation files, the APM system will use your custom translations instead of the baseline translations.
About Types of Strings in APM
- Application Strings
APM displays textual content on various user interface components such as pages, buttons, links, tiles, and so on. If a translation file is installed, the text will be displayed in the language that is based on the culture setting for the APM Security User. You can customize these translations.
- Database Strings
APM displays the database content, such as asset strategy templates, inspection recommendation content, taxonomy reference tables, help content, APM query results, and so on. The database content is not translated.
Note: The content within baseline records are not translated (for example, if we have a baseline record that contains a field, Location, and the field contains a value, the string Location is translated, but the value in that field is not translated). - Metadata Strings
APM displays the metadata content, such as datasheet captions, family captions, field captions, error messages, system codes, states, and so on. These strings appear throughout APM. If the associated translation files are installed, the metadata strings will be displayed in the language based on the culture setting for the APM Security User. By default, metadata strings are translated for all supported languages. You can customize these baseline translations.
If you create your own metadata content (for example, a new family with fields and datasheets), for each string that you use, if a baseline translation does not exist, you must provide the translation in each language in which you want the string to appear. If a string does not exist in the translation file for any language that you have installed, the string will be displayed in English to all users, regardless of their APM culture setting.
About Translatable Metadata Strings
When you create or customize metadata string translations, a custom metadata string translation file is created automatically in APM. If you want custom translations to appear in APM, you will need to upload your custom metadata string translations to the APM.
You can translate metadata strings from the following locations:
- The Manage Translations page in the Configuration Manager: From this location, you can download the baseline metadata string translations to a Microsoft Excel file, modify the translations, and then upload the Microsoft Excel file to the APM. You can also use download your custom metadata string translations, customize the translations, and then upload the modified file..
-
The Localize <Strings> window, which is accessible from the
buttons that appear throughout APM wherever you can translate a metadata string. From this location, you can add or modify metadata string translations using a grid, and they will be uploaded to APM automatically.
Custom translation files will be used instead of the baseline translation files. Because only one custom metadata string translation file can exist per language, after you create a custom metadata string translation file, if you want to make further changes, you should download your custom metadata string translation file, customize the translations, and then upload it again. The most recent file that you upload will be the file that is used by the APM system.
Metadata strings are case sensitive. This means that if the metadata string translation file contains a translated string that contains a capital letter, and you create a translation for the same string except it contains a lowercase letter, the string with the lowercase letter will be considered a new custom string (because it did not already exist in a translation file). For example, if the string, Produce (capitalized) exists in a translation file, when you create a query named produce (lowercase) and translate it, the string produce and its translations will be added to a custom translation file.
The following lists identify the metadata strings that can be translated. You can use these lists as a reference when you are translating metadata strings.
- Family captions
- Field captions
- Field help text
- Datasheet captions (standard datasheets and custom-layout datasheets)
- Datasheet section captions
- Unit of measure (UOM) captions
- System Code Table descriptions
- System Code descriptions
- Catalog item captions for all Catalog item types
- Contents of reports that is controlled by report layout (not the underlying data)
- Labels for links in the shortcut menu in query results
- Labels for a submenu in the shortcut menu in query results
- Query aliases
- Query prompt captions
- Section names in a dashboard
- Names of hyperlinks that are displayed in dashboard sections
- Labels of axes on graphs that are displayed in dashboard sections
- State captions
- State roles captions
- State operations captions
About Application String Translations
You can modify the baseline application string translations using the Manage Translations page in the Configuration Manager. On this page, you can download the baseline application string translations to a Microsoft Excel file, customize the translations, and then upload the Microsoft Excel file to the APM. When you do so, a custom application string translation file will be created automatically, and will contain all the application string translations, including your custom translations. This custom translation file will be used instead of the baseline translation file.
- Download your custom application string translation file.
- Customize the translations.
- Upload the translations again. The most recent file that you upload will be the file that is used by the APM system.
If you delete a custom application string translation file, the APM system will automatically use the baseline application string translation file.
Access the Manage Translations Page
Procedure
About the Manage Translations Application Workspace
The Application workspace on the Manage Translations page contains the following sections:
- APM Translation: Contains the following items:
- Installed Languages List: Contains the names of the non-English languages for which there are corresponding baseline application translation files on the APM system. You can use this list to determine all the non-English languages in which you can view application strings in APM.
- To download a translation file, select a language, and then in upper-right corner of the section, select
. This will download the Microsoft Excel file containing the baseline application string translations, and will then download the translations to that location from APM.
- Custom Translation: Contains the following items:
- Uploaded Languages
List: Contains the names of the non-English languages for which there are custom application translation files on APM system. If no custom application translation files exist, this list will be empty. You can use this list to determine the languages for which you have provided custom translations.
After you upload a custom application string translation file to APM, the name of the corresponding language will be added to the Uploaded Languages list. After a language appears in the Uploaded Languages list, subsequent uploads of a custom application string translation file for the same language will overwrite the custom application string translation file on the APM system with the newly uploaded file. Note that the previous file is actually moved to a different location in the APM, from which it can be restored later, if needed.
- To download, select a language, and then, in the upper-right corner of the section, select
. This will download the Microsoft Excel file containing the custom application translation file for the selected language.
- To delete a language, select a language, and then in the upper-right corner of the section, select
. A confirmation message will appear, and then the custom application translation file for the selected language will be deleted.
- Upload Custom Translations Button: Allows you to navigate to the custom application translation file containing your custom application string translations, and then upload the file to APM. After you upload a custom application string translation file to APM, the name of the language that corresponds to that file will be added to the Uploaded Languages list.
- Uploaded Languages
List: Contains the names of the non-English languages for which there are custom application translation files on APM system. If no custom application translation files exist, this list will be empty. You can use this list to determine the languages for which you have provided custom translations.
About the Manage Translations Metadata Workspace
You can use the Metadata workspace in the Manage Translations page to manage the translations for translatable metadata strings.
- APM Translation: Contains the following item:
-
Installed Languages: Contains the names of the non-English languages for which there are corresponding baseline metadata string translation files in the APM system. You can use this list to determine all the non-English languages for which you can view metadata strings in APM.
-
To download the translation file, select a language, and then in the upper-right corner of the section, select
. This will download the Microsoft Excel file containing the baseline metadata string translations, and will then download the translations to that location from APM.
-
- Custom Translations: Contains the following items:
- Uploaded languages List: Contains the names of the non-English languages for which custom metadata string translation files exist in the APM system. If no custom metadata string translation file has been uploaded to the APM, this list will be empty. You can use this list to determine the languages for which you have provided custom metadata string translations.
After you upload a custom metadata string translation file to APM, the name of the corresponding language will be added to the Uploaded Languages list. After a language appears in the Uploaded Languages list, subsequent uploads of a custom metadata string translation file for the same language will overwrite the custom metadata string translation file in the APM system with the newly uploaded file.
- To download a translation file, select a language, and then select
. This will download the Microsoft Excel file containing the custom metadata string translations for the selected language.
- To delete a language, select a language, and then in the upper-right corner of the section, select
. A confirmation message will appear, and then the custom metadata string translation file for the selected language will be deleted.
- Upload Custom Translations button: Allows you to navigate to the custom metadata string translation file containing your custom metadata string translations, and then upload the file to APM. After you upload a custom metadata string translation file to APM , the name of the language that corresponds to that file will be added to the Uploaded Languages list.
- Uploaded languages List: Contains the names of the non-English languages for which custom metadata string translation files exist in the APM system. If no custom metadata string translation file has been uploaded to the APM, this list will be empty. You can use this list to determine the languages for which you have provided custom metadata string translations.
- Custom Metadata: Contains the following items:
- Available Languages List: Contains the names of the non-English languages for which metadata string translation files exist in the APM system. You can use this list to select the languages in which you want to translate your untranslated custom metadata strings.
- Export Untranslated Metadata Button : Allows you to export your custom untranslated metadata strings to a Microsoft Excel file. Using this option, you can download and save the Microsoft Excel file containing the untranslated metadata strings.
Baseline Translations Customization Workflow
- Download the baseline metadata string translations or baseline application string translations.
- Open the Microsoft Excel file and review the translations.
- Make changes to translations as needed.
- Upload the Microsoft Excel file containing your metadata string translation changes or application string translation changes to APM.
Custom Metadata String Translation Workflow
- Export your untranslated metadata strings to a Microsoft Excel file.
- Open the Microsoft Excel file and provide translations as needed.
- Upload the Microsoft Excel file containing your translations to APM .