Reference

About the Data Loader Worksheets and Fields

Field formats for the data loader workbooks carry specific value and cell requirements. This topic contains guidelines for data/time format, units of measure (UOM), and cell color coding.

Important: When using an Excel data loader workbook, to delete rows from the workbook, you must right-click the row number and then select Delete.

Cell Color Coding

In order to differentiate between required and recommended field values in the Excel workbook, cells adhere to the following color coding scheme:

  • Red: a required field.
  • Blue: a recommended field.

Note: The Column ID and Associated Field ID will both be colored the same.

Cells that Require Logical Values

When a cell corresponds to a field in APM that requires a Logical value, you should enter True or False.

Character Limits in Character Fields

In APM, family fields that have the Character data type (Character fields) restrict values to a maximum length. In the Excel workbooks, when entering data in a cell that represents a Character field, the values must not exceed the character limit of the corresponding field.

Date and Time Format

Dates should be entered as text in the following format: YYYY-MM-DD hh:mm:ss, where:

  • YYYY is the four-digit year.
  • MM is the two-digit month.
  • DD is the two-digit day.
  • hh is hours in 24-hour notation.
  • mm is minutes.
  • ss is seconds.
Note: It is recommended to enter the dates as text in the date fields stored in the data loader workbooks.

For example, a complete entry would be the following: 2015-05-01 17:53:00. This corresponds to 5:53 PM on May 1, 2015.

Note: Hours must be entered in 24-hour notation (e.g., 17:53:00, not 5:53:00). AM and PM should never be included. Unless otherwise noted in the applicable Mappings Document, times entered should be based on the time zone of the user who will be performing the data load.”

Language

Data loader Excel workbooks are available with field captions in all baseline languages supported by APM.

Reference Sheets

You can insert additional worksheets into your data loader workbook that will not be loaded into APM by encasing the worksheet name in parentheses. For example, if you wanted to add a sheet to record notes on the data loaded into the workbook, you could add a worksheet named (Notes). Because the name of the worksheet is in parentheses, the worksheet will not be loaded into APM.

Units of Measure

In the workbooks, values that correspond to a Unit of Measure (UOM) should be entered based on the current UOM Conversion Set setting for the user performing the data load.

For example, if the UOM Conversion Set for the user is Metric, metric values should be entered in the Excel workbook.

In cells that correspond to a field that uses a UOM, you should not enter the actual UOM. For example, you should enter 10, not 10 Inches.

About the Configuration Worksheet

The Configuration Worksheet is a common worksheet, which can be implemented by each of the data loaders. It allows you to control aspects of how your data is loaded such as batching and which other worksheets should be processed.

Note: The Configuration Worksheet cannot be used by the Failure Modes and Effects Analysis (FMEA) Data Loader, the Reliability Centered Maintenance (RCM) Data Loader, Thickness Monitoring (TM) Equipment Data Loader, or the Thickness Monitoring (TM) Functional Location Data Loader.

The Configuration worksheet is needed to describe the type of data that you will be loading and how that data should be handled during the data load.

WorksheetDescription
Configuration

The Configuration worksheet is needed to describe the type of data that you will be loading and how that data should be handled during the data load.

Configuration Worksheet

Field CaptionField IDData Type (Length)Comments
Load Data From WorksheetLOAD_DATA_WORKSHEET

Boolean

Identifies if data from the corresponding worksheet identified in the Data Worksheet ID column will be loaded or not.

  • True: the corresponding worksheet will be processed.
  • False: The corresponding worksheet will not be loaded into the Meridium database.

Data Worksheet ID

DATA_WORKSHEET_ID

Character

This column contains the name of the <data> worksheet where the actual data is located. It needs to have the same name as the <data> worksheet in the data loader workbook.

Batch SizeBATCH_SIZECharacter

Modifying this field is required to determine the number of records processed in each batch. Enter the batch size you want, and the Data Loader will process that many records per batch.

For example, if you want to use a batch size of 100, enter 100, and the data loader will process 100 records per batch.

Note: The recommended batch size is 100. If the Batch Size column is removed from the source workbook, the data loader will default to a batch size of 100.

In addition to processing the data in batches, the log file reports progress by batch.

System Code Tables Used by Data Loaders

The following table lists the System Code Tables that are used by the APM Connect Data Loaders.

Table IDTable DescriptionFunction
MI_WORK_PROCESS_ADAPTERSData Loader JobsContains a list of all of the loaders and is used to link the corresponding Job Label in the APM Connect Administration Center.
MI_INTERFACE_LOG_CATEGORIES Interface log categoriesContains a list of the log categories for APM Connect, and is used to categorize the log files by APM Connect component.