Cross Domains Configuration
About Cross Domains
You can add and configure multiple domains to retrieve user information from multiple Active Directory servers to APM during the LDAP synchronization process.
Configuring Multiple Cross Domains for Synchronizing User Information
You can add and configure multiple cross domains in the Cross Domains page. The configured cross domains are used to create multiple LDAP domain records. After the LDAP domain records are created, using the LDAP synchronization process, you can retrieve the user information for the Microsoft Active Directory users associated with the Microsoft Active Directory domains that have been defined in APM.
Note: If Single Sign-On (SSO) authentication is enabled for the users to access APM, you can use only one cross domain to retrieve user information from the associated Active Directory server using the LDAP synchronization process.
Access the Cross Domains Page
Procedure
In the module navigation menu, select
.
The Cross Domains page appears.