Content Validation
Enable Content Validation
About This Task
When content validation is enabled, each time a user navigates to Configuration Manager, a check will be performed to ensure that the baseline APM content is valid. If the content is not valid, it will display a warning message. The user will have the option of exporting the invalid content or ignoring the warning.
Procedure
About Accessing APM When Content Validation is Enabled
About This Task
When you navigate to Configuration Manager in which Content Validation has been enabled, the APM system will scan the database for invalid content. If invalid content in detected, the following warning message will be displayed.
When this warning message is displayed, you have two options for how to proceed:
- You can select Yes to check the invalid content. This option is recommended. When you select this option, the Content Validation page appears, displaying a list of invalid content in the Content Summary section.
- You can select the No to bypass the warning and continue using the application anyway. Using a system that contains invalid content is not recommended.