Workflow
APM Strategy: Asset Strategy Optimization Workflow
This workflow describes the process of determining the optimal strategy for a piece of equipment or location using additional features from ASM, which can then be viewed and managed further in ASM.
In the following workflow diagram, the blue text in a shape indicates that a corresponding description has been provided in the sections that follow the diagram. For more information, refer to the topic Interpreting the Workflow Diagrams.
Asset Strategy Management (ASM)
Persona: Analyst
Strategies that are generated by ASM can be analyzed in ASO to compare scenarios and propose the optimal strategy to complete the ASM workflow.
Go to the ASM workflow.
Modify Analysis Parameters
Persona: Analyst
Modify values as needed in the appropriate fields for the Analysis.
Create Scenario
Persona: Analyst
Create Active, Proposed, and additional scenarios.
Modify Scenario
Persona: Analyst
Modify risks and actions.
Run Simulation
Persona: Analyst
Run a simulation to assemble possible scenarios based on the strategy.
Set Scenario as Proposed
Persona: Analyst
Set the scenario as proposed and select Run Simulation again to export back to ASM.
Review Results/Compare Scenarios
Persona: Analyst
Review and compare the results of the simulated scenarios to determine the best scenario for your specific case.