Implement Actions from System Strategy

Access the Implement Workspace

Procedure

  1. Access the ASM Overview page.
  2. Select the System Strategies tab.
    The System Strategies section appears, displaying a list of available system strategies.
  3. Select the system strategy whose actions you want to implement.
    The Strategy Summary workspace for the selected system strategy appears.

  4. Select the Implement tab.
    The Implement workspace appears.

Create New Measurement Location or Lubrication Requirement Records

About This Task

In the Implement workspace, you can create corresponding measurement location and lubrication requirement records to implement an action. After you create the records, you can link to them from the Implement workspace.

Procedure

  1. Access the Implement workspace.
  2. In the Implement workspace, select the check box in the row containing the action you want to implement via a new Measurement Location or Lubrication Requirement record.
    The action is highlighted.
  3. Select the Implement drop-down menu, and then select Measurement Location or Lubrication Requirement.
    The Implement Lubrication Requirement window or the Implement Measurement Location window appears, depending on which type of implementation you selected, displaying a list of measurement location or lubrication requirement records from Rounds to which you could link the action.

  4. Select the Create New option.
    A grid appears, displaying a list of available template types.
  5. Select the template type you want to use, and then select Implement.
    A message appears, confirming that the action has been implemented successfully.

Results

  • A new measurement location or lubrication requirement is created.
  • In the Implement workspace, in the Implementation column of the action you implemented, a hyperlink to the measurement location or lubrication requirement appears.

Create EAM Maintenance Plan Record

About This Task

In the Implement workspace, you can create corresponding EAM maintenance plan record to implement an action.

Procedure

  1. Access the Implement workspace.
  2. In the Implement workspace, select the check box in the row containing the action you want to implement via a new EAM maintenance plan record.
    The actions are highlighted.
  3. Select the Implement drop-down menu, and then select EAM Maintenance Plan.
    The Implement as EAM Maintenance Plan window appears.

  4. Select Create New, and then select Implement.
    A message appears, confirming that the action has been implemented.

Results

  • The new EAM plan is created.
  • In the Implement workspace, in the Implementation column of the action you implemented, a hyperlink to the EAM maintenance plan appears.

Apply Updates to Implemented Actions

Before You Begin

  • Modify action(s) as necessary for the asset strategy that is linked to your system strategy. When you do so, the state assignment for the strategy is changed to Modified.

Procedure

  1. Approve the strategy whose related actions you modified.
    The strategy is changed back to the Active state.
  2. Access the Implement workspace.

  3. In the Implement workspace, select the actions that you modified and you want to update with their implementations, and then select .
    The updates are applied to the implemented actions. If any updates were unsuccessful, the Errors window appears, which contains a list of the unsuccessful updates.

Send Approved Actions to an ASI Package

Procedure

  1. Access the Implement workspace.
  2. In the Implement workspace, select the check box in the rows containing the implemented actions that you want to send to ASI, and then select .
    The Send to ASI Package window appears, displaying a list of existing implementation packages that match the CMMS system of the Asset. By default, the Link Existing option is selected.

    Note:
    • The maximum amount of records that you can select for one implementation is 250.
    • The button will be enabled only if one of the following conditions are satisfied:
      • The Asset is an equipment or a functional location.
      • The Asset has a CMMS system.
  3. If you want to send the implemented actions to an existing ASI package, select the package to which you want to link them, and then select Send. Or, if you want to create a new ASI package and link the implemented actions to an existing ASI package, select Create New, then enter values in the available fields as needed, and then select Send.
    A message appears, confirming that your items have been sent to ASI.

Delete a System Strategy

Procedure

  1. Access the ASM Overview page.
  2. Select the System Strategies tab.
    The System Strategies section appears, displaying a list of system strategies.
  3. Select the row containing the strategy that you want to delete, and then, in the section, select .
    The Confirm Delete dialog appears, asking you to confirm that you want to delete the strategy.
  4. Select Yes.
    The strategy is deleted.
    Note: You can also delete a strategy using the delete button () under option while viewing the strategy that you want to delete.