SIL Validation
SIS Management: SIL Validation Workflow
This workflow describes the process of validating the function of the safety equipment (sensors, logic solvers, and final elements) installed to safeguard an instrumented function.
In the following workflow diagram, the blue text in a shape indicates that a corresponding description has been provided in the sections that follow the diagram. For more information, refer to the topic Interpreting the Workflow Diagrams.

Define Proof Test Template
Persona: Analyst
Create a Proof Test Template and Proof Test Template Details to specify the trip points and error limits for each element in the PIL.
Approve Proof Test Template
Persona: Analyst
Approve the Proof Test Template by selecting Approved in the Template Status field.
Define Proof Test Task
Persona: Analyst
Create a Proof Test Task record to schedule the proof test and assign the task to a user. You can also use Inspection Tasks (of the type Proof Test) created in Asset Strategy Management, which are listed in the Proof Test Tasks section of the SIS Management Overview page.
Perform Proof Test
Persona: Technician
Print the Proof Test Template. Perform the proof test in the field as per the instructions provided in the Proof Test Template.
Enter Proof Test Results and Complete Proof Test
Persona: Technician
Create a Proof Test to enter the readings taken while performing the proof test in the field. Link the Proof Test to the Proof Test Template and the Proof Test Task. GE Digital APM indicates whether each step in the proof test has passed or failed.
Review, Approve, and Close Proof Test
Persona: Analyst
Review the proof test results, and then close it by selecting Closed in the Functional Test Status field.
Create Recommendation
Persona: Analyst
You can create a Recommendation to provide suggestions to improve the proof test results or to prevent overt failures such as broken electrical conduit, failure of a protective element, rusted wires, or the presence of excess moisture.
Promote to ASM
Persona: Analyst
Promote the Recommendation to Asset Strategy Management (ASM), where the associated action can be implemented as an Inspection Task of the task type Proof Test.
Asset Strategy Management
Persona: Analyst
Go to the Asset Strategy Management workflow.
SIL Assessment
Persona: Analyst
Go to the SIL Assessment workflow.
SIL Verification
Persona: Analyst
Go to the SIL Verification workflow.