Family Field Descriptions
ACA Records
The following table provides an alphabetical list and description of the fields that exist in the ACA family. The information in the table reflects the baseline state and behavior of these fields.
This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. For more information, refer to the Sites section of the documentation.
Field | Data Type | Description | Behavior and Usage |
---|---|---|---|
Analysis Description | Character | A description of the ACA. | None |
Analysis End Date | Date | The date on which the ACA will end. | None |
Analysis ID | Character | The ID for the ACA. | This field is required, and the value must be unique. |
Analysis Owner | Character | The name of the team member who is specified as the Process Owner for the ACA. | This field is disabled and populated automatically with the value in the Process Owner field. |
Analysis Scope | Text | A description of the ACA that you want to conduct. | None |
Analysis Start Date | Date | The date on which the ACA will begin. | None |
Analysis Type | Character | N/A | By default, this field does not appear on the ACA datasheet. |
Facilitator | Character | The name of the team member who is specified as the Facilitator for the ACA. | By default, this field does not appear on the ACA datasheet. This field is populated automatically with the name of the ACA team member specified as the Facilitator in the ACA Team Members section. |
Imported By | Character | The user ID of the Security User who created or last updated the analysis from a Microsoft Excel file. | This field is disabled and populated automatically when you create an analysis or update the risk values by importing data from an Excel file. |
Import Date | Date | The date on which the analysis was created or last updated from a Microsoft Excel file. | This field is disabled and populated automatically when you create an analysis or update the risk values by importing data from an Excel file. |
Import Status | Character | The status of the import process that was last used to create or update the analysis. |
This field is disabled and populated automatically when you create an analysis or update the risk values by importing data from an Excel file. Tip: For more information, refer to the Data Loaders section of the documentation.
The value will be set to one of the following:
The status is also displayed in the grid on the ACA Import page. |
Last Modified By | Character | The name of the user who last modified the record. | This field is disabled and populated automatically with the name of the user who was logged in when the record was last modified. |
Last Modified Date | Date | The date on which the record was last modified. | This field is disabled and populated automatically. |
Process Owner | Character | The name of the Process Owner for the ACA. | By default, this field does not appear on the ACA datasheet. It is populated automatically with the name of the ACA team member specified as the Process Owner in the ACA Team Members section. When a user creates a new ACA record, this value defaults to the name of the user who created the record. After a team member has been assigned to the role of Process Owner, this field will be updated automatically with that team member's name. |
Visual Attributes | Text | N/A | By default, this field does not appear on the ACA datasheet. |
Criticality Records
Criticality records store assessment data to allow future expanded criticality options and assessment features. This topic provides an alphabetical list and description of the fields that exist for the Criticality family. The information in the table reflects the baseline state and behavior of these fields.
Field | Data Type | Description | Behavior and Usage |
---|---|---|---|
Assessment | Text | Stores a serialized JSON representation of criticality that has been assessed using the Risk Matrix or Criticality Matrix tool. | This is a system field. |
Assessment Method | Text | Describes how criticality was assessed. | A system field that contains one of the following values:
|
Asset Key | Numeric | The Entity Key of the asset. | None |
Basis for Assessment | Character | A brief summary of the rationale used to assess criticality. | This field is automatically populated with the value you enter in the Basis for Assessment field. |
Threshold Key | Numeric | The numeric key indicating the label and color associated with the threshold value. | A numeric key that determines the label and color associated with the Criticality record. It is also a foreign key to the Criticality Threshold family. |
Value | Numeric | Stores the canonical criticality value for a given asset. | The value in this field is used as the basis for computing the Criticality Definition threshold. |
Criticality Checklist Records
This family is a template for assessing criticality with the Criticality Checklist. This topic provides an alphabetical list and description of the fields that exist for the Criticality family. The information in the table reflects the baseline state and behavior of these fields.
Field | Data Type | Description | Behavior and Usage |
---|---|---|---|
Basis for Assessment | Text | Provides details about the Criticality Assessment. | This field is automatically populated with the value you enter in the Basis for Assessment field. |
Environment Consequence | Character | Assesses the environmental consequence of the Criticality Checklist item. | Populated automatically from the criticality value assessed from the environmental effects of an asset. |
Operations Consequence | Character | Assesses the operations consequence of the Criticality Checklist item. | Populated automatically from the criticality value assessed from the operational effects of an asset. |
PM Required | Boolean | Indicates whether or not preventive maintenance is required. | If the value in this field is true, then the asset requires preventive maintenance. |
Safety Consequence | Character | Assesses the safety consequence of the Criticality Checklist item. | Populated automatically from the criticality value assessed from the safety effects of an asset. |
Criticality Definition Records
Criticality Definition records store references to the criticality thresholds and assessment options. It also enables the user to modify assessment methods. This topic provides an alphabetical list and description of the fields that exist for the Criticality Definition family. The information in the table reflects the baseline state and behavior of these fields.
Field | Data Type | Description | Behavior and Usage |
---|---|---|---|
Checklist Family | Character | The family ID of the Criticality Checklist family used for assessment. | If the Use Checklist check box is selected, then the family indicated in this field will be required. |
Default | Boolean | Indicates whether or not this is the default Criticality Definition. | You can specify only one Criticality Definition record as the default. In the Standard Practice Criticality Definition record, the Default check box is cleared. In the Default Criticality Definition record, the Default check box is selected. |
Name | Character | The name of the Criticality Definition. | This value is used to identify the record and must be unique. In the baseline Criticality Definition record, the Criticality Definition name is Default. |
Use Checklist | Boolean | Indicates whether or not to use the Criticality Checklist Assessment method. | If this check box is selected, then this will be used, and this will be required. |
Criticality Threshold Records
Criticality Threshold records store the threshold bands that define a criticality definition. This topic provides an alphabetical list and description of the fields that exist for the Criticality Threshold family. The information in the table reflects the baseline state and behavior of these fields.
Field | Data Type | Description | Behavior and Usage |
---|---|---|---|
Color | Character | The color of the criticality badge. | None |
Description | Character | The description of the criticality value. | None |
Value | Numeric | A number that represents the threshold level associated with the criticality value. | This value is the lower limit for a given threshold. |