GE’s focus on safety at the site includes initiatives such as the “Stop Work Authority,” which gives power to employees to stop production if they identify a work hazard. In addition, rigorous quarterly audits and a permit-to-work process, activities such as daily site work coordination, toolbox talks, walkdowns, inspections and reward programs are implemented on a regular basis to aim to ensure safety remains top of mind.
The full balance of plant will comprise one generating block, equipped with one of GE’s 7HA.02 gas turbines powering an H65 generator, a STF-A650 steam turbine powering an H33 generator, and a heat recovery steam generator.
The expanded plant, which is planned to begin operation in 2021, will add an additional capacity of 550 MW. In Taiwan, GE Vernova continues to play a critical role in supporting the advancement of the country’s energy goals, working alongside customers such as Chiahui Corporation. GE Vernova is strongly positioned to help the country support its mission to increase natural gas to 50% of the energy mix. The project serves as a significant achievement in supporting the government’s goals to phase out nuclear power, and increase capacity by 30 GW by 2025.