Powering Tomorrow

Where the Next Generation of Energy Technology Comes to Life

By Alasdair Lane | July 17, 2026

ARC outside grand opening
arc ribbon cutting

Today’s energy grid faces increasingly powerful pressures both new and old, from AI data centers to aging and inefficient equipment. Combined, they are putting an unprecedented strain on global energy systems. At the same time, promising emerging technologies can’t be implemented until they can prove they work, at scale, outside the laboratory. Finding solutions to these challenges is the aim of GE Vernova’s Advanced Research Center (ARC) in Niskayuna, New York. The newly expanded Frontier Campus, an applied research and testing facility, aims to help accelerate the transition from lab breakthroughs to real-world energy solutions.

The ARC Frontier Campus opened with a celebration on July 16, following a $110 million joint investment with the State of New York. The center is expected to create 75 new research positions. During the celebration, visitors were allowed to tour the laboratories and explore the ARC’s work on data-center power, robotics, advanced materials, carbon removal, and atmospheric water harvesting.  

    Meeting the Demands of AI

    By 2030, AI data centers could account for 9% of the electricity generated in the U.S., up from 4% in 2025. Securing that supply while limiting emissions will be essential, though it addresses only part of the engineering problem. AI-related computing loads often change abruptly, forcing the equipment behind them to react within microseconds while remaining coordinated. Developing systems capable of handling those rapid fluctuations will require sustained investment in research and manufacturing — which is why GE Vernova plans to spend $11 billion on capital expenditure and research and development through 2028. 

    At Niskayuna, that investment is supporting work on modernizing both the wider energy grid and the components within it. The site’s researchers are using digital models and physical controls to re-create the behavior of a data center before equipment is installed. They’re also refining the controls inside solid-state transformers, which use semiconductors and software to manage electricity more precisely than conventional equipment. 

    That precision is critical in a hyperscale data center, where tens of thousands of power-conversion elements must react almost instantly without falling out of step with one another. Quicker, more predictable controls can help manage sudden changes in computing activity while delivering more power from a smaller footprint. 

    GE Vernova's Headquarters in Cambridge, MA

    Two Years In

    The world’s demand for energy is growing at a pace that’s increasingly difficult to match, and GE Vernova is meeting the challenge head-on.

    Mike Englert standing in front of board of wires

    Better Brains

    Meet the engineer helping to power complex new AI data centers.

    2030

    AI data centers could account for 9% of the electricity generated in the U.S., up from 4% in 2025.

    Building Smarter, More Resilient Infrastructure

    The main issues facing aging infrastructure include an increased need for faster and more timely inspections, reducing risks, preventing downtime, and extending asset life. The ARC is addressing all of them, and more, to strengthen reliability across the energy system, whether through robotics, high-tech materials, or increased recyclability.   

    For example, a wind turbine blade can take around 2,000 labor hours to produce, yet small flaws inside its structure are difficult to spot before it leaves the factory. Teams at Niskayuna are training computer vision models on tens of thousands of annotated images so robotic systems can examine blade interiors and guide human reviewers toward areas that need closer attention. 

    Similar tools are being used inside operating power facilities. Four-legged robots developed with ANYbotics — a company specializing in autonomous inspection machines — can climb stairs, enter confined areas, and collect visual, thermal, acoustic, and gas readings in places where heat, high voltage. or restricted access can make human inspection dangerous. In one trial, AI models reviewed 400 images of bolts, flanges, and pipe surfaces in 30 minutes, as compared with an estimated two weeks for a manual review. Repeated visits can also reveal how equipment is changing over time, helping engineers detect early signs of wear before they lead to lost output or an unplanned shutdown. 

    Materials research addresses reliability even earlier, during the design and manufacture of the equipment itself. At the Frontier Campus, specialists are using scanning technology to study how metals behave under stress, while computational methods help narrow the search for compositions suited to demanding conditions. 

    Those decisions can affect a component long after it enters service. A 62-meter wind blade developed by ZEBRA, an industry research consortium focused on recyclable turbine blades, uses a thermoplastic resin that allows its main materials to be separated and recycled at the end of its working life.  

    wind turbine blades

    Blade Runners

    GE Vernova is deploying AI-enabled machines to boost wind turbine blade quality.


    Dog robot partnership with ANYbotics and GE Vernova

    Power Couple

    How GE Vernova and ANYbotics are transforming energy industry asset inspections.

    Vernova Image

    Closing the Loop

    Group unveils a prototype of a recyclable wind turbine blade.

    30 minutes

    In one trial, AI models reviewed 400 images of bolts, flanges, and pipe surfaces in 30 minutes, where a manual review would take an estimated two weeks.

    Advancing a More Sustainable and Accessible Energy Future

    Other teams are converting science into practical tools for decarbonization, resilience, and access. For instance, some work with sorbents, materials that bind with selected molecules from the surrounding air. A practical application for these is direct air capture, which collects and concentrates carbon dioxide so it can be stored or used. A pilot unit at Niskayuna can remove 10 metric tons of CO₂ a year. Engineers are testing a stronger sorbent that could raise that figure to between 30 and 40 metric tons using the same rig, alongside improvements intended to reduce the energy consumed during the process. 

    The same underlying science is being applied to water. AirJoule — an atmospheric water-harvesting system — draws moisture from the atmosphere and releases it as distilled, potable water. It was developed through a program run by the United States Defense Advanced Research Projects Agency, which backs high-risk research with practical potential. The refrigerator-size technology is now being commercialized for military and humanitarian use, industrial dehumidification, and commercial air-conditioning. 

    A man stands in a lab site with helmet and yellow vest

    Out of Thin Air

    Meet the engineer working to remove CO2 from the atmosphere.

    Air2Water model

    DARPA AIR2WATER Project

    GE Vernova’s Advanced Research Center successfully concludes independent verification and validation milestone

     Arc opening demo

    The ARC’s Frontier Campus gives researchers more room to test these emerging technologies under real-world conditions while also working through the practical barriers that determine whether they can succeed at scale. That means the ARC can be a bridge across the gap between invention and deployment, as well as an accelerator — so the technologies needed to modernize the grid are better, stronger, and available for implementation faster.