Reporting Nonconformance
Manufacturing floor operators create nonconformance records when they are working on a part that may not meet quality standards.
Clock onto an operation.
- Click the Report Nonconformance tab.
- For serialized parts only, select a serial number.Only the clocked-on serial numbers appear, and you can report non-conformance on one serial number at a time.
- Keep the Auto-Generate Name check box selected (default setting), or clear the check box to enable the field, then enter a name. If you keep the default setting the field remains disabled, since it is already populated with the work order name.
- For nonserialized parts only, enter the affected quantity in the Quantity field.The available quantity is shown in parentheses on the right.
- From the Defect Category drop-down list, select the category that best fits the reason for nonconformance.
- If you selected Failed Measurements, a second drop-down list appears. Select the applicable reason.
- In the Description field, describe the nonconformance issue.
- If a long explanation is required, use the Additional Details field.
- If custom properties have been configured in PM MES, the fields appear below the Additional Details field. Enter applicable values. Note: If you use the wrong format, an error message appears.
- Click Report Non-Conformance.A status message appears to confirm that the record was created.
- Optional: Repeat this procedure to create another nonconformance record.