Ingest Assets through the User Interface for Legacy Predix APM
Before You Begin
Important: You must ingest the enterprise, site, segment, and asset data using the Asset Ingestion Loader ( ). For more information on using the Asset Ingestion Loader, refer to Unified Loaders documentation in the About Data Loaders section of the help.
Important:
You must have the Asset ZIP file containing one or more valid JSON files. You must have access to the Asset Ingestion module in your application.In Predix APM, adding or modifying assets using the Legacy Predix APM user interface, APIs, or Asset Ingestion Service, or bypassing the Unified Asset Ingestion Data Loader, causes the asset databases to become out-of-sync.
In Predix APM:
- You must add or modify assets using the Unified Asset Ingestion Data Loader.
- You cannot delete assets.
- You must use the Asset Ingestion Service to add tags to assets.
In Legacy Predix APM:
- You can add, modify, or delete assets in the user interface, using APIs, or using the Asset Ingestion Service.
- You can add tags to assets in the user interface, using APIs, or using the Asset Ingestion Service.
About This Task
Ingest only the following asset data through the user interface:
- Reserved attributes
- Custom attributes
- Geo location
- Groups
- Tags
- Classifications
Important:
- When ingesting classifications, instances, connections, tagClassifications, and tagAssociations as separate files, you must ingest the <your_classifications_filename>.zip file first. You can then repeat this procedure to ingest each of the remaining files in the following order: <your_instances_filename>.zip, <your_connections_filename>.zip, <your_tagClassfications_filename>.zip, and <your_tagAssociations_filename.zip>.
- If you ingest data with an existing id the new data replaces the existing data in GE Digital APM. This applies all data types.
The following limitations exist for asset ingestion:
- Same file cannot be reingested until completed. Unless, the file has been in progress for more than 30 minutes.
- Ingestion zip file size is limited to 10 MB.
The following table displays a summary of the last 100 ingestions:
Field | Description |
---|---|
File Name | Displays the name of the ingestion file. |
Status | Displays the status of the ingestion. The status can be any of the following:
|
Task Progress | Displays the percentage of the ingestion. |
Start Time | Displays the date and time the ingestion started. |
End Time | Displays the date and time the ingestion ended. |
File Size | Displays the size of the ingestion file. |
Procedure
Results
Legend | Description |
---|---|
Completed | The ingestion completed successfully. You should be able to see the ingested asset data in the Assets module. |
Completed with Errors | The ingestion completed with errors. Review the error(s) for details and possible resolution. Some of these errors can be related to data validation issues. |
In Progress | The file ingestion into the application asset store is currently in progress. Ingested assets will be available in the application after the ingestion completes. |
Skipped | The file ingestion was skipped due to the file being already in progress from a previous ingestion. Wait for the previous ingestion to complete or wait 30 minutes to re-ingest the file. |