There is one associated with Thickness Monitoring: tm. The following table describes the various paths that build on the route, and the elements that you can specify for each.
Element | Description | Accepted Value(s) | Notes |
---|---|---|---|
tm/unit: Opens the Thickness Monitoring Overview workspace. tm/unit/<UnitEntityKey>: Displays the selected unit on the Thickness Monitoring Overview workspace. |
|||
<UnitEntityKey> | Specifies the Functional Location or Unit you want to view in TM. | Any Entity Key that corresponds to a Unit or Functional Location. | Required. |
tm/asset/<AssetEntityKey>: Displays the selected asset in the Analysis Overview workspace. tm/asset/<AssetEntityKey>/settings: Displays the selected asset in the Corrosion Analysis Settings workspace. tm/asset/<AssetEntityKey>/input: Displays the selected asset in the Measurement Data Entry workspace. |
|||
<AssetEntityKey> | Specifies the asset you want to view in TM. | Any Entity Key that corresponds to an asset. | Required. |
tm/asset/<AssetEntityKey>/subcomponent/<TMLGroupEntityKey>: Displays the selected TML Group in the Analysis Overview workspace. tm/asset/<AssetEntityKey>/subcomponent/<TMLGroupEntityKey>/settings: Displays the selected TML Group in the Corrosion Analysis Settings workspace. tm/asset/<AssetEntityKey>/subcomponent/<TMLGroupEntityKey>/input: Displays the selected TML Group in the Measurement Data Entry workspace. |
|||
<TMLGroupEntityKey> | Specifies a TML Group linked to an asset that you want to view in TM. | Any Entity Key that corresponds to a TML Group. | Required. |
tm/asset/<AssetEntityKey>/tml/<TMLEntityKey>: Displays the selected TML in the Analysis Overview workspace. tm/asset/<AssetEntityKey>/tml/<TMLEntityKey>/settings: Displays the selected TML in the Corrosion Analysis Settings workspace. |
|||
<UnitEntityKey> | Specifies a TML linked to an asset that you want to view in TM. | Any Entity Key that corresponds to a TML. | Required. |
Example URL | Destination |
---|---|
tm/unit |
The Thickness Monitoring Overview workspace. |
tm/unit/2305330 | The Thickness Monitoring Overview workspace for the specified unit. |
tm/asset/2509505 | The Analysis Overview workspace for the specified asset. |
tm/asset/2509505/settings | The Corrosion Analysis Settings workspace for the specified asset. |
tm/asset/2509505/input | The Measurement Data Entry workspace for the specified asset. |
tm/asset/2509505/subcomponent/3476094 | The Analysis Overview workspace for the TML Group with Entity Key 3476094, which is linked to the asset with Entity Key 2509505. |
tm/asset/2509505/subcomponent/3476094/settings |
The Corrosion Analysis Settings workspace for the TML Group with Entity Key 3476094, which is linked to the asset with Entity Key 2509505. |
tm/asset/2509505/subcomponent/3476094/input |
The Measurement Data Entry workspace for the TML Group with Entity Key 3476094, which is linked to the asset with Entity Key 2509505. |
tm/asset/2509505/tml/6225073 | The Analysis Overview workspace for the TML with Entity Key 6225073, which is linked to the asset with Entity Key 2509505. |
tm/asset/2509505/tml/6225073/settings |
The Corrosion Analysis Settings workspace for the TML with Entity Key 6225073, which is linked to the asset with Entity Key 2509505. |
Copyright © 2018 General Electric Company. All rights reserved.