About Thickness Monitoring Tasks

Thickness Monitoring Tasks can be used to manage the inspection schedules for assets that you analyze in TM. Thickness Monitoring Task records will be created automatically when you create Corrosion Analysis Settings for an asset or TML Group. If you select the Auto Manage Tasks check box on the TM Admin Preferences page, when you update a TML, the corresponding Thickness Monitoring Task will be updated automatically.

The Auto Manage Tasks setting is disabled by default. If the Risk Based Inspection license is active, you should accept the default setting because you will use the Tasks generated from RBI, rather than TM, to determine your inspection intervals. If the Risk Based Inspection license is not active, you should enable the Auto Manage Tasks setting.

Note: Thickness Monitoring will create and update Thickness Monitoring Tasks automatically only if the Component ID setting is defined for the Equipment or TML Group family.

Copyright © 2018 General Electric Company. All rights reserved.