This following table provides a list of default settings for each datalogger. You must review them and modify if needed before sending or receiving data from a datalogger.
Datalogger | Connection Type | Baud Rate | COM Port | Datalogger Service Port |
---|---|---|---|---|
GE DMS Go | USB | N/A | N/A | 2014 |
GE DMS Go+ | USB | N/A | N/A | 2014 |
GE DMS2 | Serial | Per Device Setting | COM1 | 2014 |
Olympus (Panametrics) 37DL Plus Ultrasonic Thickness Gage | Serial | 1200 | COM1 | 2014 |
Olympus (Panametrics) 38DL Plus Ultrasonic Thickness Gage | USB | N/A | N/A | 2014 |
Note: The Olympus (Panametrics) 38DL Plus Ultrasonic Thickness Gage also supports the serial connection type. When you set the Connection Type to Serial, the Olympus (Panametrics) 38DL Plus Ultrasonic Thickness Gage uses the same default settings as the Olympus (Panametrics) 37DL Plus Ultrasonic Thickness Gage.
Copyright © 2018 General Electric Company. All rights reserved.