License Requirements
This feature is available with the core GE Digital APM application; no specific license is required.
Additional Components Required
In addition to the basic GE Digital APM system architecture, the following additional components are required:
R Server: A machine on which the R Server software is installed. The software requirements of this server are determined by the third-party distributor of the software. You can find more information about this software, including required software dependencies and installation instructions, on the R Server website.
The GE Digital APM testing environment uses DeployR Open 8.0.0 and DeployR Enterprise 8.0.0.
Note: The World Wide Web Publishing service must be enabled on the R Server in order to use R scripts in GE Digital APM. If this setting is disabled during the installation of R Server, you must enable it.
Deploying R Scripts
After you have installed and configured the basic GE Digital APM system architecture, you will need to perform some configuration steps specifically for R Scripts.
Supported Features in
All standard GE Digital APM product features for this module are available in the
Copyright © 2018 General Electric Company. All rights reserved.