License Requirements
This feature is available in the GE Digital APM application with the Meridium Core license; no specific license is required.
ACA integration with SAP is only available in on-premises releases.
To update your SAP system to reflect the criticality value that is determined in ACA, the licenses SAP Interfaces – Foundation and SAP Interfaces - Criticality Assessment are also required.
Note: For supported SAP releases, see the SAP System Requirements section in APM Connect System Requirements.
Additional Components Required
Only the basic GE Digital APM system architecture is required for this feature to work correctly. No additional components are required.
Deploying Asset Criticality Analysis
After you have installed and configured the basic GE Digital APM system architecture, you will need to perform some configuration steps specifically for Asset Criticality Analysis.
Supported Features in
All standard GE Digital APM product features for this module are available in the
Copyright © 2018 General Electric Company. All rights reserved.