LDAP Field Mapping Records

This topic provides an alphabetical list and description of the fields that exist in LDAP Field Mapping records. The information in the table reflects the baseline state and behavior of these fields.

Field Data Type Description Behavior and Usage
LDAP Field Character The name of Microsoft Active Directory field that will serve as the source for the mapping. For each LDAP field that you want to map to a GE Digital APM field, you must define the LDAP field manually You can obtain a list of available Active Directory fields from Microsoft.
Meridium Field Character The field ID of the field in GE Digital APM that will serve as the target field for the mapping. For each GE Digital APM field to which you want an LDAP field to map, you must define the GE Digital APM field manually. The field can belong to any family, but you will probably want to specify a field that is defined in the Human Resource family or the Security User family. Be sure to specify the field ID, not the field caption.

Copyright © 2018 General Electric Company. All rights reserved.