LDAP Domain Records

This topic provides an alphabetical list and description of the fields that exist in Domain records. The information in the table reflects the baseline state and behavior of these fields.

Field Data Type Description Behavior and Usage
Caption Character A short description of the domain. You can define this value manually to help distinguish this domain from any other domains that you define.
Default Site Character The default site that will be assigned to new Security Users created during LDAP synchronization. None
Name Character The name of the domain. You must define this value manually and should include the domain extension (e.g., domain.com). The value that you specify in this field will be used in conjunction with the @ symbol and Microsoft Active Directory user names to create GE Digital APM Security User IDs. For example, if a user's name is jsmith and the domain extension is example.com, the GE Digital APM Security User ID for that user would be [email protected].
Root Character The starting point of the container in which GE Digital APM will look for user objects in Microsoft Active Directory. The GE Digital APM system will use this information to find user objects in Microsoft Active Directory.
User Filter Character This filter is used to locate users within the specified directory. This filter is used during the synchronization process to locate Microsoft Active Directory users that belong to a specific group within the domain. You can accept the default value in this field.

Copyright © 2018 General Electric Company. All rights reserved.