Classifier Training History records store the ratings specified by users when they train a machine learning script (i.e., classifier) in the Test Results workspace of the script. This topic provides an alphabetical list and description of the fields that exist for the Classifier Training History family. The information in the table reflects the baseline state and behavior of these fields.
This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.
Field |
Data Type |
Description |
Behavior and Usage |
---|---|---|---|
Classifier |
Character |
The machine learning script (i.e., classifier) that was trained. |
This field is populated automatically. |
Prediction |
Character |
The prediction provided by the classifier. |
This field is populated automatically. |
Standard List |
Character |
The standard list used by the classifier. |
This field is populated automatically. |
Training Date |
Date |
The time in UTC when the classifier was trained. |
This field is populated automatically. |
Training Text |
Text |
The cleaned text that was used by the classifier to determine a prediction. |
This field is populated automatically. |
Training User |
Character |
The ID of the user who trained the classifier. |
This field is populated automatically. |
User Value |
Character |
The correct value as specified by the user. |
When the prediction is a Boolean, the User Value is determined based on the User Vote applied to the Prediction. For example, if the classifier predicted True, and the user votes that the prediction is incorrect, the User Value is specified as False automatically. This field is populated automatically. |
User Vote |
Boolean |
The user’s indication of whether the classifier’s prediction was correct or incorrect. |
This value is specified when the user selects This field is populated automatically. |
Copyright © 2018 General Electric Company. All rights reserved.