About Script Score

The score of a prediction produced by a machine learning or fuzzy logic script represents the goodness of fit, in the statistical sense, for the specific prediction. When testing a script, scores are presented as a percentage between 0.0% and 100.0%. When passing the script score to a successor node in a Cognitive Analytics cognition, scores are presented as a numeric value between 0 and 1. Higher scores mean that the prediction, according to the script's logic, is more likely to be a correct prediction.

Copyright © 2018 General Electric Company. All rights reserved.