This topic provides an alphabetical list and description of the fields that exist for the Software family and appear on the Software datasheet, unless otherwise specified. The information in the table reflects the baseline state and behavior of these fields.
Field |
Data Type |
Description |
Behavior and Usage |
---|---|---|---|
Is Default | Logical | Indicates whether the record is the default one. | If set true, then the SRS Template is a default template for the category supplied by GE Digital. |
Last Modified By | Character | The name of the user who last modified the record. | On the datasheet, this field is disabled and updated automatically whenever the record is modified. |
Last Modified Date | Date | The date on which the record was last modified. | On the datasheet, this field is disabled and populated automatically. |
Revision Number | Numeric | A number that represents the number of times the record has been revised. | On the datasheet, this field is disabled and populated. |
SIS Firmware 61508 Certificate | Text | Certificate location and certifying agency for the SIS firmware (typically from exida or TUV) | On the datasheet, this field appears as a text box, in which you can enter the certifying agency for the SIS firmware, as well as the location and validity of the certificate. |
SIS Firmware Version | Text | The firmware version of the SIS from the OEM. | On the datasheet, this field appears as a text box, in which you can enter the firmware version for the SIS firmware, typically supplied by the OEM. |
SIS Maintenance Software Name | Text | The name of the SIS maintenance software (for example: GE ToolboxST) | On the datasheet, this field appears as a text box, in which you can enter the name and version of the SIS maintenance software and other licensing details. |
SIS Maintenance Software Version Number | Text | The software version compatible with the SIS hardware. | On the datasheet, this field appears as a text box, in which you can enter the version of the SIS maintenance software compatible with the SIS hardware. |
SIS Programming Software Name | Text | The name of the SIS maintenance software (for example: GE ToolboxST) | On the datasheet, this field appears as a text box, in which you can enter the name and version of the SIS programming software and other licensing details. |
SIS Programming Software Version Number | Text | The software version compatible with the SIS hardware. | On the datasheet, this field appears as a text box, in which you can enter the version of the SIS programming software compatible with the SIS hardware. |
SIS Software Requirements | Text | The workstation and other platform requirements for the software. | On the datasheet, this field appears as a text box, in which you can enter the workstation and other platform requirements (such as Windows 10 profession version) for the SIS maintenance software and SIS programming software. |
SRS Template Description | Character | A description of the record. | On the datasheet, this field appears as a text box labeled Description, in which you can enter a description of the record. |
SRS Template ID | Character | The ID of the record. | On the datasheet, this field appears as a text box labeled Field ID, in which you can type the ID. |
Copyright © 2018 General Electric Company. All rights reserved.