This topic provides an alphabetical list and description of the fields that exist for the Operations family and appear on the Operations datasheet, unless otherwise specified. The information in the table reflects the baseline state and behavior of these fields.
Field |
Data Type |
Description |
Behavior and Usage |
---|---|---|---|
Interlocks that are used for bypassing SIFs during start up or other operations |
Text |
The interlock used to bypass the SIF during startup or other unique operations such as proof testing. | On the datasheet, this field appears as a text box, in which you can enter the interlocks bypass design basis (used during startup, proof testing or overrides). |
Is Default | Logical | Indicates whether the record is the default one. | If set true, then the SRS Template is a default template for the category supplied by GE Digital. |
Last Modified By | Character | The name of the user who last modified the record. | On the datasheet, this field is disabled and updated automatically whenever the record is modified. |
Last Modified Date | Date | The date on which the record was last modified. | On the datasheet, this field is disabled and populated automatically. |
Revision Number | Numeric | A number that represents the number of times the record has been revised. | On the datasheet, this field is disabled and populated. |
SIF Bypass Requirements | Text | The bypass requirements the SIF during startup or other unique operations such as proof testing. | On the datasheet, this field appears as a text box, in which you can enter the SIF bypass design basis (used during startup, proof testing or overrides). |
SIF Manual Shutdown | Text | The method of manually shutting down an SIF. | On the datasheet, this field appears as a text box, in which you can enter the methodology to manually shut down SIF. (during emergency situations). |
SIF Proof Test Interval | Text | The proof test interval. | On the datasheet, this field appears as a text box, in which you can enter the proof testing interval (for example 24 months). |
SIF Start Up Requirements | Text | The sequence and method of starting up an SIF. | On the datasheet, this field appears as a text box, in which you can enter the sequence and method of startup of a SIF. |
SRS Template Description | Character | A description of the record. | On the datasheet, this field appears as a text box labeled Description, in which you can enter a description of the record. |
SRS Template ID | Character | The ID of the record. | On the datasheet, this field appears as a text box labeled Field ID, in which you can type the ID. |
Copyright © 2018 General Electric Company. All rights reserved.